L3.10.53 Xorg xrandr command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

L3.10.53 Xorg xrandr command

Jump to solution
3,267 Views
torus1000
Contributor V

Hi Chip experts,

According to the document, xrandr command already supported.

     i.MX_6_Graphics_Users_Guide.pdf

     https://community.freescale.com/message/520370

So I tried to change --brightness or --gamma of my SabreSD board but nothing changed.

Have those xrandr parameters been supported?

If somebody knows, please let me know. Please see attached log.

Thanks.

root@imx6dlsabresd:~# export DISPLAY=:0.0

root@imx6dlsabresd:~# xrandr --output "DISP3 BG - DI1" --brightness 0.5

root@imx6dlsabresd:~# xrandr --output "DISP3 BG - DI1" --gamma 1.5:1.5:1.5

root@imx6dlsabresd:~# xrandr --verbose

Screen 0: minimum 240 x 240, current 1024 x 768, maximum 8192 x 8192

DISP3 BG - DI1 connected 1024x768+0+0 (0x40) normal (normal left inverted right x axis y axis) 0mm x 0mm

        Identifier: 0x3f

        Timestamp:  1838592668

        Subpixel:   unknown

        Gamma:      1.0:1.0:1.0

        Brightness: 0.0

        Clones:

        CRTC:       0

        CRTCs:      0

        Transform:  1.000000 0.000000 0.000000

                    0.000000 1.000000 0.000000

                    0.000000 0.000000 1.000000

                   filter:

  U:1024x768p-60 (0x40)   65.0MHz -HSync -VSync -CSync *current +preferred

        h: width  1024 start 1064 end 1124 total 1344 skew    0 clock   48.4KHz

        v: height  768 start  775 end  785 total  806           clock   60.0Hz

root@imx6dlsabresd:~# xrandr -o left

root@imx6dlsabresd:~# xrandr -o right

root@imx6dlsabresd:~# xrandr -o inverted

root@imx6dlsabresd:~# xrandr -o normal

root@imx6dlsabresd:~# xrandr -s 1920x1080

Size 1920x1080 not found in available modes

root@imx6dlsabresd:~# xrandr -s 1024x768

Labels (2)
0 Kudos
Reply
1 Solution
2,689 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi torus1000,

Current xrand is supported however there are some features that are not accelerated by GPU, and this is marked as a bug.

Reduced graphic performance with rotated screen (imx6, sabresd)

Hope this helps

View solution in original post

0 Kudos
Reply
2 Replies
2,690 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi torus1000,

Current xrand is supported however there are some features that are not accelerated by GPU, and this is marked as a bug.

Reduced graphic performance with rotated screen (imx6, sabresd)

Hope this helps

0 Kudos
Reply
2,688 Views
chandrasekharma
Contributor III

root@sabresd_6dq:/ # export DISPLAY=:0.0
root@sabresd_6dq:/ # xrandr
/system/bin/sh: xrandr: not found
127|root@sabresd_6dq:/ # xrandr left                                           
/system/bin/sh: xrandr: not found
127|root@sabresd_6dq:/ # echo $DISPLAY
:0.0
root@sabresd_6dq:/ # export DISPLAY=0
root@sabresd_6dq:/ # xrandr
/system/bin/sh: xrandr: not found
127|root@sabresd_6dq:/ #

I am getting above errors please confirm me. and xrandr bin not visbile in /system/bin/. Please help me to run xrandr

0 Kudos
Reply