L2.6.35_11.01.00_ER_source_bundle.tar.gz build failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

L2.6.35_11.01.00_ER_source_bundle.tar.gz build failed

1,277件の閲覧回数
neeveehariharan
Contributor I

Hi,

I have downloaded "L2.6.35_11.01.00_ER_source_bundle.tar.gz" and done the instructions as per IMX53_Start_linux_bsp_userguide.pdf". I am getting lots of errors during the compilations.

It seems that "www.bitshrine.org" does not necessary files needed.

I got error like "mtdutils, linux-2.6.35.3.tar.b2, linux-2.6.35_imx" lots of files are missing in the repository.

I have also cross checked that the "L2.6.35_11.01.00_ER_source_bundle.tar.gz" fully downloaded.

Since we are struck here, we require your valuable inputs in this regards,

Thanks,
Hariharan.V.

ラベル(1)
0 件の賞賛
返信
0 返答(返信)