L2.6.35_11.01.00_ER_source_bundle.tar.gz build failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

L2.6.35_11.01.00_ER_source_bundle.tar.gz build failed

1,278 Views
neeveehariharan
Contributor I

Hi,

I have downloaded "L2.6.35_11.01.00_ER_source_bundle.tar.gz" and done the instructions as per IMX53_Start_linux_bsp_userguide.pdf". I am getting lots of errors during the compilations.

It seems that "www.bitshrine.org" does not necessary files needed.

I got error like "mtdutils, linux-2.6.35.3.tar.b2, linux-2.6.35_imx" lots of files are missing in the repository.

I have also cross checked that the "L2.6.35_11.01.00_ER_source_bundle.tar.gz" fully downloaded.

Since we are struck here, we require your valuable inputs in this regards,

Thanks,
Hariharan.V.

Labels (1)
0 Kudos
Reply
0 Replies