Kitkat AOSP with Linux kernel 4.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kitkat AOSP with Linux kernel 4.1

1,578 Views
lajeshd
Contributor I

Hi Guys,

Is it possible to use linux kernel 4.1 with kitkat AOSP on sabresd board ?

If so could you please share the git url of linux kernel 4.1 bsp ?

Do you have any reference document for this process ?

Thanks,

Lajesh D

Labels (1)
0 Kudos
Reply
1 Reply

1,470 Views
b36401
NXP Employee
NXP Employee

We have do any document for such backporting.
Sorry for the inconvenience.

I suppose it is possible to implement.
However it will be a manual process that will require rebuilding the desired Android version from the AOSP using the kernel you need.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply