Key generation for encrypted boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Key generation for encrypted boot

Jump to solution
2,932 Views
friederbaumgrat
Contributor III

Dear NXP community,

I am currently working on the encrypted boot for IMX.6 CPUs.

Everything works, but I have one problem. I have to encrypt the same image and transfer them to different boards (same CPU). The current state is, that I run the CST Tool and transfer the generated output key (dek.bin) to the board and call the dek_blob function in order to generate the dek_blob.bin (final key).

Is there a way I don't need to transfer the dek.bin to the board?

Is is possible to generate the dek_blob.bin on my host computer?

Best regards,

Frieder

Labels (1)
0 Kudos
Reply
1 Solution
2,504 Views
gary_bisson
Senior Contributor III

Hi,

No there is no way, that is the whole point of the process, to be unique per board since it relies on each board unique ID/key.

If you really want to flash the exact same image on each platform, I guess you'll need give up on encryption and sign only.

Regards,

Gary

View solution in original post

2 Replies
2,505 Views
gary_bisson
Senior Contributor III

Hi,

No there is no way, that is the whole point of the process, to be unique per board since it relies on each board unique ID/key.

If you really want to flash the exact same image on each platform, I guess you'll need give up on encryption and sign only.

Regards,

Gary

2,504 Views
friederbaumgrat
Contributor III

Hey Gary,

Thank you for your answer.

Regards,

Frieder

0 Kudos
Reply