Kernel port build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel port build error

2,930 Views
michealbrenad
Contributor I

I am having 3.14 working kernel for my imx6quad ,i want to port 3.10 to imx6q , during the build process i am getting the following error, and am i stuck, please help to rectify the problem.

i am using the same boradconfig and dtb patch file form 3.14.

arch/arm/mach-imx/built-in.o: In function `imx6sl_enter_wait':

platform-spi_imx.c:(.text+0x246c): undefined reference to `ultra_low_bus_freq_mode'

platform-spi_imx.c:(.text+0x2470): undefined reference to `audio_bus_freq_mode'

arch/arm/mach-imx/built-in.o: In function `imx6sx_enter_wait':

platform-spi_imx.c:(.text+0x259c): undefined reference to `low_bus_freq_mode'

arch/arm/mach-imx/built-in.o: In function `mu_work_handler':

platform-spi_imx.c:(.text+0x5278): undefined reference to `request_bus_freq'

platform-spi_imx.c:(.text+0x52a4): undefined reference to `release_bus_freq'

arch/arm/mach-imx/built-in.o: In function `imx6sl_set_wait_clk':

platform-spi_imx.c:(.text+0x6610): undefined reference to `low_bus_freq_mode'

platform-spi_imx.c:(.text+0x6614): undefined reference to `audio_bus_freq_mode'

arch/arm/mach-imx/built-in.o: In function `imx6sl_cpuidle_init':

platform-spi_imx.c:(.init.text+0x4194): undefined reference to `imx6sl_low_power_wfi'

platform-spi_imx.c:(.init.text+0x41a0): undefined reference to `mx6sl_lpm_wfi_start'

platform-spi_imx.c:(.init.text+0x41a4): undefined reference to `mx6sl_lpm_wfi_end'

arch/arm/mach-imx/built-in.o: In function `imx6sx_cpuidle_init':

platform-spi_imx.c:(.init.text+0x4468): undefined reference to `imx6sx_low_power_idle'

platform-spi_imx.c:(.init.text+0x446c): undefined reference to `mx6sx_lpm_wfi_start'

platform-spi_imx.c:(.init.text+0x4470): undefined reference to `mx6sx_lpm_wfi_end'

arch/arm/mach-imx/built-in.o: In function `imx6q_map_io':

platform-spi_imx.c:(.init.text+0x8c08): undefined reference to `imx6_busfreq_map_io'

arch/arm/mach-imx/built-in.o: In function `imx6sl_map_io':

platform-spi_imx.c:(.init.text+0xb758): undefined reference to `imx6_busfreq_map_io'

arch/arm/mach-imx/built-in.o: In function `imx6sx_map_io':

platform-spi_imx.c:(.init.text+0xfbb0): undefined reference to `imx6_busfreq_map_io'

drivers/built-in.o: In function `imx6_pcie_host_init':

vf610_adc.c:(.text+0x229a4): undefined reference to `request_bus_freq'

vf610_adc.c:(.text+0x229f8): undefined reference to `release_bus_freq'

vf610_adc.c:(.text+0x22a68): undefined reference to `request_bus_freq'

drivers/built-in.o: In function `mxc_epdc_fb_runtime_resume':

vf610_adc.c:(.text+0x40cd0): undefined reference to `request_bus_freq'

drivers/built-in.o: In function `mxc_epdc_fb_runtime_suspend':

vf610_adc.c:(.text+0x40ce4): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `mxsfb_runtime_resume':

vf610_adc.c:(.text+0x48c24): undefined reference to `request_bus_freq'

drivers/built-in.o: In function `mxsfb_runtime_suspend':

vf610_adc.c:(.text+0x48c4c): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `pxp_runtime_resume':

vf610_adc.c:(.text+0x4f5e4): undefined reference to `request_bus_freq'

drivers/built-in.o: In function `pxp_runtime_suspend':

vf610_adc.c:(.text+0x4f60c): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `regulator_disable':

vf610_adc.c:(.text+0x57668): undefined reference to `set_cpufreq_lock'

drivers/built-in.o: In function `regulator_enable':

vf610_adc.c:(.text+0x577cc): undefined reference to `set_cpufreq_lock'

drivers/built-in.o: In function `ahci_imx_error_handler':

vf610_adc.c:(.text+0xeb8c4): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `imx_ahci_suspend':

vf610_adc.c:(.text+0xeb924): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `imx6q_sata_exit':

vf610_adc.c:(.text+0xeb97c): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `imx_ahci_resume':

vf610_adc.c:(.text+0xebd88): undefined reference to `request_bus_freq'

drivers/built-in.o: In function `imx6q_sata_init':

vf610_adc.c:(.text+0xebef4): undefined reference to `request_bus_freq'

drivers/built-in.o: In function `fec_runtime_resume':

vf610_adc.c:(.text+0x13a43c): undefined reference to `request_bus_freq'

drivers/built-in.o: In function `fec_runtime_suspend':

vf610_adc.c:(.text+0x13a450): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `imx_controller_resume':

vf610_adc.c:(.text+0x1a5ef0): undefined reference to `request_bus_freq'

vf610_adc.c:(.text+0x1a5f0c): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `imx_controller_suspend':

vf610_adc.c:(.text+0x1a605c): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `ci_hdrc_imx_remove':

vf610_adc.c:(.text+0x1a61d0): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `ci_hdrc_imx_probe':

vf610_adc.c:(.text+0x1a646c): undefined reference to `request_bus_freq'

vf610_adc.c:(.text+0x1a6488): undefined reference to `release_bus_freq'

vf610_adc.c:(.text+0x1a6724): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `sdhci_esdhc_runtime_resume':

vf610_adc.c:(.text+0x24b78c): undefined reference to `request_bus_freq'

drivers/built-in.o: In function `sdhci_esdhc_runtime_suspend':

vf610_adc.c:(.text+0x24b7f8): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `sdhci_esdhc_imx_probe':

vf610_adc.c:(.text+0x24c294): undefined reference to `request_bus_freq'

vf610_adc.c:(.text+0x24c2a0): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `gpu_runtime_resume':

vf610_adc.c:(.text+0x255900): undefined reference to `request_bus_freq'

drivers/built-in.o: In function `gpu_runtime_suspend':

vf610_adc.c:(.text+0x255914): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `ipu_runtime_resume':

vf610_adc.c:(.text+0x27332c): undefined reference to `request_bus_freq'

drivers/built-in.o: In function `ipu_runtime_suspend':

vf610_adc.c:(.text+0x273340): undefined reference to `release_bus_freq'

drivers/built-in.o: In function `vpu_runtime_resume':

vf610_adc.c:(.text+0x289084): undefined reference to `request_bus_freq'

drivers/built-in.o: In function `vpu_runtime_suspend':

vf610_adc.c:(.text+0x289098): undefined reference to `release_bus_freq'

sound/built-in.o: In function `fsl_ssi_runtime_resume':

last.c:(.text+0x2e90c): undefined reference to `request_bus_freq'

sound/built-in.o: In function `fsl_ssi_runtime_suspend':

last.c:(.text+0x2e920): undefined reference to `release_bus_freq'

sound/built-in.o: In function `fsl_spdif_runtime_resume':

last.c:(.text+0x3179c): undefined reference to `request_bus_freq'

sound/built-in.o: In function `fsl_spdif_runtime_suspend':

last.c:(.text+0x317b0): undefined reference to `release_bus_fre

please help..

Labels (4)
0 Kudos
Reply
3 Replies

2,203 Views
michealbrenad
Contributor I

Thanks igorpadykov ,

i have one more doubt can i use the dts file from the kernel 3.14 to 3.10 with out any porting effort. My understanding is dts file is board dependent it just passes the hardware info to the kernel. Is that correct ?

0 Kudos
Reply

2,203 Views
igorpadykov
NXP Employee
NXP Employee

Hi Micheal

I think you are right

~igor

0 Kudos
Reply

2,203 Views
igorpadykov
NXP Employee
NXP Employee

Hi Micheal

for 3.10.x one can look at nxp L3.10.17 sources

linux-2.6-imx.git - Freescale i.MX Linux Tree

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply