Kernel header files for imx8mqevk.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kernel header files for imx8mqevk.

1,640件の閲覧回数
axue
Contributor I

Hi,

I need to build my device driver on an imx8mqevk. Now it is running kernel 5.15.5-lts-next+gc1084c2773fc, where could I download kernel headers?

Thanks,

Adam

 

0 件の賞賛
返信
3 返答(返信)

1,627件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

We don't provide header for download.

The header will be generated in yocto building process.

0 件の賞賛
返信

1,619件の閲覧回数
axue
Contributor I

Hi Qmiller,

I made a yocto build, still not sure which folder contains the right kernel header files.

Tried to use /build-wayland/tmp/work-shared/imx8mqevk/kernel-source, but the compile failed.

ERROR: Kernel configuration is invalid.
include/generated/autoconf.h or include/config/auto.conf are missing.
Run 'make oldconfig && make prepare' on kernel src to fix it.

Thanks,

Adam

 

0 件の賞賛
返信

1,613件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Qmiller_0-1652170404061.png

Find this folder

0 件の賞賛
返信