Kernel for 8MPLUS-BB Evalboard with 8MPLUS-LPD4-CPU-Module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel for 8MPLUS-BB Evalboard with 8MPLUS-LPD4-CPU-Module

2,391 Views
steffendoster
Contributor IV

Hello everyone,

I'm stuck here with an 8MPLUS-BB Evalboard together with an 8MPLUS-LPD4-CPU-Module.

All I want is to compile a linux-kernel and devicetree which is able to display something on HDMI.

Sadly I had to realize that the board and the imx8mplus-evk.dts aren't fully compatible and that the board uses a LVDS-to-HDMI-Bridge which also isn't available in the kernel (https://github.com/Freescale/linux-fslc).

Am I using the wrong Kernel? Which one is the correct kernel to properly bring up all the features of the board? Where can I get the sources for this board?

0 Kudos
Reply
3 Replies

2,378 Views
khang_letruong
Senior Contributor III

Hi @steffendoster 

The official kernel for iMX platforms can be found here : https://source.codeaurora.org/external/imx/linux-imx/

The latest release seems to be lf-5.10.52-2.1.0, and you can find the dts of 8MPLUS EVK here : https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale?h=lf-5.10.52.... Possibly it is one of imx8mp-ddr4-evk.dts or imx8mp-evk.dts.

Hope that helps,
Khang

0 Kudos
Reply

2,342 Views
steffendoster
Contributor IV

Hi Khang,

yes, this was a great help. Thank you.

I downloaded and compiled the i.MX-Kernel and HDMI ran out of the box. Nice.
I hope the necessary drivers and devicetrees will find their way into mainline-kernel as well.

Greetings

Steffen

0 Kudos
Reply

2,363 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Good!

0 Kudos
Reply