Kernel crash with 3.0.35

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kernel crash with 3.0.35

1,372 次查看
sivaalagarsamy
Contributor II

I am running linux 3.0.35 on a custom imx6 board. On some boards after a day of running fine, the kernel crashes. It seems to happen only if I enable a wifi module (realtek 8192cu).

There are other instances of the same board running fine with the wifi module.

Here is the crash log on the console. The stack info seems to indicate an issue with memory.

Any one has any thoughts on why this might be happening?

Unable to handle kernel NULL pointer dereference at virtual address 00000003

pgd = ba4c4000

[00000003] *pgd=4fdc3831, *pte=00000000, *ppte=00000000

Internal error: Oops: 817 [#4] PREEMPT SMP

Modules linked in: 8192cu ftdi_sio

CPU: 2    Tainted: G      D      (3.0.35-1.0.0 #1)

PC is at get_page_from_freelist+0x148/0x5c0

LR is at zone_watermark_ok+0x20/0x28

pc : [<800b4978>]    lr : [<800b31c4>]    psr: 600f0093

sp : bfb05d98  ip : 00000000  fp : 00000001

r10: 00000000  r9 : 805f3c00  r8 : bfb04000

r7 : 0bfe7000  r6 : 805f3c00  r5 : 8bff4570  r4 : 80035150

r3 : 00200200  r2 : 00100100  r1 : 8c01c15c  r0 : ffffffff

Flags: nZCv  IRQs off  FIQs on  Mode SVC_32  ISA ARM  Segment user

Control: 10c53c7d  Table: 4a4c404a  DAC: 00000015

Process deckard (pid: 1567, stack limit = 0xbfb042f0)

Stack: (0xbfb05d98 to 0xbfb06000)

5d80:                                                       00000041 00000001

5da0: bffd1700 ffffffff 600f0013 8c01c15c 00000000 805bdcc8 00020200 00000000

5dc0: 00000020 805f46e4 bfb05e44 00000000 00000000 00000000 00000000 bfb05e80

5de0: bfb04000 bfb04000 00000001 ffffffff 805fc438 805f3c00 0000010d 805f46e0

5e00: 00000000 805f3c00 00000001 00000000 805bdb40 805f46e4 00000200 800b549c

5e20: 00000001 00000041 805f3c00 00000000 bfb05e44 00000000 00000000 00020200

5e40: 00000001 805fc438 00000000 bffbfa00 bffd1780 00000010 00000000 00000002

5e60: 00000000 00000000 00000000 00000000 00000800 00000000 8c018ee0 bffbfa00

5e80: 00000064 805f3c00 bfb05e84 bfb05e8c 3496ca18 00000001 00000001 00000000

5ea0: bfb4fba0 bfb05ef8 37724000 ba583478 00000000 37726000 37726000 800b5aec

5ec0: 00000008 800c91fc 00000001 00000001 00000000 00000000 bfb4fba0 00000000

5ee0: 00000000 80031ee0 bffbd220 00000000 00000008 bfb05ef8 bfb05fac 8043a2f4

5f00: 37724000 00002000 bfb4fbdc 8043c2b0 805bdcc8 805aa040 37724000 ba583478

5f20: 37726000 00000000 00000004 bfb04000 bfb04000 800c6b74 001a08a8 00000001

5f40: 00000000 00000081 001a08a8 00000001 001a09c4 80095ef8 3496ca18 00000000

5f60: 00000000 00000000 ba583478 bfb04000 805bdcc8 80031c00 00000102 bfb04000

5f80: 805bdcc8 37703020 37700000 00022fe0 000000dc 80039284 bfb04000 00000000

5fa0: 00024000 80039100 37703020 37700000 37724000 00002000 00000004 00000000

5fc0: 37703020 37700000 00022fe0 000000dc 2de00010 00002000 2de00010 00024000

5fe0: 00001000 3496c96c 4ab99cec 4abf380c 600f0010 37724000 00000000 00000000

[<800b4978>] (get_page_from_freelist+0x148/0x5c0) from [<800b549c>] (__alloc_pages_nodemask+0xe8/0x728)

[<800b549c>] (__alloc_pages_nodemask+0xe8/0x728) from [<800b5aec>] (__get_free_pages+0x10/0x24)

[<800b5aec>] (__get_free_pages+0x10/0x24) from [<800c91fc>] (zap_page_range+0x54/0x14c)

[<800c91fc>] (zap_page_range+0x54/0x14c) from [<800c6b74>] (sys_madvise+0x394/0x578)

[<800c6b74>] (sys_madvise+0x394/0x578) from [<80039100>] (ret_fast_syscall+0x0/0x30)

Code: e5950018 e3402010 e3a03c02 e3403020 (e5801004)

---[ end trace 72bc50fe04348d0b ]---

标签 (3)
0 项奖励
回复
1 回复

1,067 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Siva

wifi module may consume much current and introduce

additional board noise which affects memory. One can try to

increase wifi power supply current capability, add filtering capacitors,

inprove wifi module shielding. For testing one can decrease board operating

frequency (this will decrease board noise) and slightly increase power supply

voltage of ddr memory. Ferrite beads may be recommended on wifi module

power cables for decreaseing emi.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复