Kernel choice

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,462件の閲覧回数
angelo_d
Senior Contributor I

Hi all,

for imx6q-plus have to decide if to use 3.14.52 or 4.1.15.

We actually uses 2 screens, with a 2D app in one + a 3D app in the second.

I am not sure if is more mature the (34.1.14) p8.4 vivante driver compared to p7.4 (3.14.52).

And, it there is any other reason to prefer one or the other.

Many thanks

angelo

ラベル(1)
0 件の賞賛
返信
1 解決策
3,280件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Angelo

please refer to attached L4.1.15 Release Notes Table 9 New features

describing new features and bug fixes for the graphics provided in this release,

compared with L3.14.52 previous version.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
3,281件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Angelo

please refer to attached L4.1.15 Release Notes Table 9 New features

describing new features and bug fixes for the graphics provided in this release,

compared with L3.14.52 previous version.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

3,280件の閲覧回数
angelo_d
Senior Contributor I

Hi Igor, many thanks !

I have kernel 4.1.15 running, once added vivante gpu libraries (5.1.1 p8.3)  3D and 2D demos works fine.

0 件の賞賛
返信