Kernel boot logo on HDMI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel boot logo on HDMI

1,710 Views
clemntnxp
Contributor I

Hello,

I want to have my kernel boot logo and yocto psplash screen centered on HDMI connected panel.

Currently, logos are mapped from the top left corner of my HDMI panel.

From LVDS it looks OK because my logo size fit my LVDS screen size.

Any idea ?

0 Kudos
Reply
2 Replies

1,653 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

I suggest you check the next link on section "Splash Screen position":

Splash Screen on U-Boot | Toradex Developer Center

Best regards.

0 Kudos
Reply

1,620 Views
clemntnxp
Contributor I

Hello Jorge,

 

yes i already see this topic but it's about u-boot and I'm talking about kernel boot logo and yocto psplash screen.

Thanks

0 Kudos
Reply