Kernel boot logo on HDMI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kernel boot logo on HDMI

1,684件の閲覧回数
clemntnxp
Contributor I

Hello,

I want to have my kernel boot logo and yocto psplash screen centered on HDMI connected panel.

Currently, logos are mapped from the top left corner of my HDMI panel.

From LVDS it looks OK because my logo size fit my LVDS screen size.

Any idea ?

0 件の賞賛
返信
2 返答(返信)

1,627件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

I suggest you check the next link on section "Splash Screen position":

Splash Screen on U-Boot | Toradex Developer Center

Best regards.

0 件の賞賛
返信

1,594件の閲覧回数
clemntnxp
Contributor I

Hello Jorge,

 

yes i already see this topic but it's about u-boot and I'm talking about kernel boot logo and yocto psplash screen.

Thanks

0 件の賞賛
返信