Kernel authentication issue with HAB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kernel authentication issue with HAB

2,710件の閲覧回数
ganesh_k
Contributor III

Hi All,

         I m trying to implement secure boot on imx6ulevk
https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/habv4/guides/mx6_mx7_secure_boot.t...

with help of above document, I can able to sign and authenticate uboot with fuse as open, below is the log for hab_status:

=> hab_status

Secure boot disabled

HAB Configuration: 0xf0, HAB State: 0x66
No HAB Events Found!

=>

 Now I tried to sign and authenticate Linux fitImage, fitImage is authenticating and loading properly.
Below is the boot log:

switch to partitions #0, OK
mmc1(part 0) is current device
switch to partitions #0, OK
mmc1(part 0) is current device
10542944 bytes read in 267 ms (37.7 MiB/s)
Booting from mmc ...
10542944 bytes read in 267 ms (37.7 MiB/s)
hab fuse not enabled

Authenticate image from DDR location 0x83000000...

Secure boot disabled

HAB Configuration: 0xf0, HAB State: 0x66
No HAB Events Found!

## Loading kernel from FIT Image at 83000000 ...
   Using 'conf-imx6ul-pds.dtb' configuration
   Verifying Hash Integrity ... OK
   Trying 'kernel-1' kernel subimage
     Description:  Linux kernel
     Type:         Kernel Image
     Compression:  uncompressed
     Data Start:   0x830000e0
     Data Size:    10504440 Bytes = 10 MiB
     Architecture: ARM
     OS:           Linux
     Load Address: 0x80800000
     Entry Point:  0x80800000
     Hash algo:    sha256
     Hash value:   1b7abd41dffe4ae2dfb9e9a17c016c680539a791ef61010a4b70d3b481237fc8
   Verifying Hash Integrity ... sha256+ OK
## Loading fdt from FIT Image at 83000000 ...
   Using 'conf-imx6ul-pds.dtb' configuration
   Verifying Hash Integrity ... OK
   Trying 'fdt-imx6ul-pds.dtb' fdt subimage
     Description:  Flattened Device Tree blob
     Type:         Flat Device Tree
     Compression:  uncompressed
     Data Start:   0x83a04ae4
     Data Size:    32036 Bytes = 31.3 KiB
     Architecture: ARM
     Hash algo:    sha256
     Hash value:   7fd68eccd6a191a0d69f70fb7c08d30b208cba93aa15186804697db4c84af7fe
   Verifying Hash Integrity ... sha256+ OK
   Booting using the fdt blob at 0x83a04ae4
   Loading Kernel Image
   Using Device Tree in place at 83a04ae4, end 83a0f807
ft_system_setup for mx6

Starting kernel ...

Details:

fitImage loadaddress = "0x83000000"
fitImage size              = "0xA0CB3C"
padded fitImage size = "0xA0D000"

genIVT file:

#! /usr/bin/perl -w
use strict;
open(my $out, '>:raw', 'ivt.bin') or die "Unable to open: $!";
print $out pack("V", 0x412000D1); # IVT Header
print $out pack("V", 0x83000000); # Jump Location
print $out pack("V", 0x0); # Reserved
print $out pack("V", 0x0); # DCD pointer
print $out pack("V", 0x0); # Boot Data
print $out pack("V", 0x83A0D000); # Self Pointer
print $out pack("V", 0x83A0D020); # CSF Pointer
print $out pack("V", 0x0); # Reserved
close($out);

but when I try to authenticate fitImage from uboot with hab_auth_img, im getting the below error:

=> load mmc 1 0x83000000 fitImage-without-ramfs_signed.bin
10542944 bytes read in 267 ms (37.7 MiB/s)
=> hab_auth_img 0x83000000 0xA0D000
hab fuse not enabled

Authenticate image from DDR location 0x83000000...
Error: CSF lies outside the image bounds

 Please suggest me if I m doing something wrong.



Thanks & Regards

Ganesh.K

ラベル(2)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,419件の閲覧回数
_sanath_
Contributor II

Hello,

I am facing the same issue with iMX8mm evk board.

Did you find any working solution for this?

Any inputs from @igorpadykov is much appreciated.

 

Thanks and regards

Sanath

0 件の賞賛
返信

2,662件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ganesh

 

internal team notified me that this issue is already considered internally.

 

Best regards
igor

0 件の賞賛
返信