Kernel Version for iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kernel Version for iMX6

5,246件の閲覧回数
richogrady
Contributor II

Freescale has several kernel versions that support iMX6.  What is the best kernel version to use as far as support for iMX6 features?

ラベル(2)
0 件の賞賛
返信
1 返信

3,379件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Rich,

it may be difficult to define a best version. Naturally the newest version should be the best option, but there are always patches required, then after some time the latest version is released it becomes stable.

Please note that there are BSPs for i.MX processors developed by NXP and there are also BSPs created by a community external to NXP such as the one you are referring to.

You can find the NXP BSPs releases here: git.freescale.com > fsl-arm-yocto-bsp.git

On the other hand the BSPs releases developed by the external community can be found here: https://github.com/Freescale/

If you are using a board based on our Reference Designs and Evaluation Boards you may use our BSP, in this case imx-4.1-krogoth

But if you are using a custom board and it is not based on our reference Designs you may use a BSP developed by the community, in this case branch Morty would be the indicated.

just please be aware that NXP provides support of the BSPs developed by NXP, but unfortunately the releases of the external community are out of our scope.


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信