Kernel Source code 3.14.52 for imx6 sabresd

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kernel Source code 3.14.52 for imx6 sabresd

3,662 次查看
sijilpu
Contributor I

Hi

    I am trying to upgrade the kernel version 3.0 to 3.14 (for linux) in imx sabresd . I need  a kernel source code for this and   also want   to know the procedure for doing this. can you please provide the link for the kernel source code(3.14) that will support in imx6 sabresd board.

Thanks

标签 (3)
0 项奖励
回复
2 回复数

2,238 次查看
art
NXP Employee
NXP Employee

Please refer to the attached document for the detailed information on how to install, build and deploy the 3.14.52 Linux BSP for i.MX6 series processors.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,238 次查看
gary_bisson
Senior Contributor III

Hi,

Here is the official repo:

linux-2.6-imx.git - Freescale i.MX Linux Tree

You should use this tag for 3.14:

linux-2.6-imx.git - Freescale i.MX Linux Tree

Note that 4.1.15 is now available too.

Regards,

Gary

0 项奖励
回复