Kernel Panic on Pre-Built Linux SDCard image for MCIMX8M-EVK: Evaluation Kit?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kernel Panic on Pre-Built Linux SDCard image for MCIMX8M-EVK: Evaluation Kit?

4,241件の閲覧回数
glen_m_cornell
Contributor I

It appears that the pre-built Linux SDcard image for the #i.MX 8M evaluation kit downloaded from the NXP website fails with a kernel panic.  Is anyone else seeing the same thing?

We recently purchased the MCIMX8M-EVK: Evaluation Kit for the i.MX 8M Applications Processor, downloaded the pre-built Linux BSP (https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_MX8MQ&appType=license&Parent_nodeId=151310... ), and performed the following, according to the documentation:

  1. extracted the L4.9.88_2.0.0_images_MX8MQ.tar.gz tarball (md5sum: e7fd9c911d12bf3807bba3b040eb0f2a)

    tar zxvf L4.9.88_2.0.0_images_MX8MQ.tar.gz

  2. decompressed the SD card image: 

    cd L4.9.88_2.0.0_images_MX8MQ

    bunzip2 fsl-image-qt5-validation-imx-xwayland-imx8mqevk.sdcard.bz2

  3. Copied the image to an SD card:

    sudo dd if=fsl-image-qt5-validation-imx-xwayland-imx8mqevk.sdcard of=/dev/mmcblk0

I placed the SDcard in the evaluation board, set the jumpers for the proper boot, and applied power to the card.  I found two problems.  First, the monitor showed nothing on the screen (the monitor indicated that it received no signal).  "systemctl status" indicated no error with any processes. 2. The kernel panicked about 4 minutes into the boot process (output of serial port is attached):

[ 242.786648] INFO: task systemd-udevd:2801 blocked for more than 120 seconds.
[ 242.793723] Tainted: G O 4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d #1
[ 242.801430] "echo 0 > /proc/sys/kernel/hung_task_timeout_secs" disables this message.
[ 242.809452] systemd-udevd D 0 2801 1771 0x0000020d
[ 242.815083] Call trace:
[ 242.817544] [<ffff000008085e98>] __switch_to+0x90/0xc0
[ 242.822810] [<ffff000008c653f0>] __schedule+0x178/0x590
[ 242.828159] [<ffff000008c65844>] schedule+0x3c/0xa8
[ 242.833157] [<ffff000008c688e4>] schedule_timeout+0x174/0x248
[ 242.839025] [<ffff000008c67680>] __down+0x58/0x90
[ 242.843852] [<ffff000008102e74>] down+0x4c/0x68
[ 242.849478] [<ffff000000f4155c>] HIFExchangeBMIMsg+0x20c/0x330 [wlan]
[ 242.856971] [<ffff000000f47ac4>] bmi_download_firmware+0x64/0x130 [wlan]
[ 242.864708] [<ffff000000edff9c>] vos_open+0x174/0x6c0 [wlan]
[ 242.871378] [<ffff000000d9bca4>] hdd_wlan_startup+0x5ac/0x12e0 [wlan]
[ 242.878462] [<ffff000000f45cc8>] hif_pci_probe+0x5f8/0x858 [wlan]
[ 242.884685] [<ffff000008486c4c>] pci_device_probe+0x9c/0x140
[ 242.890461] [<ffff000008649a40>] driver_probe_device+0x1d0/0x2c8
[ 242.896580] [<ffff000008649bf4>] __driver_attach+0xbc/0xc0
[ 242.902181] [<ffff000008647b34>] bus_for_each_dev+0x4c/0x98
[ 242.907867] [<ffff0000086493b8>] driver_attach+0x20/0x28
[ 242.913294] [<ffff000008648fa8>] bus_add_driver+0x1b8/0x228
[ 242.918976] [<ffff00000864a578>] driver_register+0x60/0xf8
[ 242.924576] [<ffff0000084857a8>] __pci_register_driver+0x38/0x40
[ 242.931321] [<ffff000000f45630>] hif_register_driver+0x18/0x38 [wlan]
[ 242.938482] [<ffff000000d93d80>] hdd_hif_register_driver+0x30/0x78 [wlan]
[ 242.946002] [<ffff0000012010b4>] hdd_module_init+0xb4/0x1000 [wlan]
[ 242.952416] [<ffff000008083a50>] do_one_initcall+0x38/0x130
[ 242.958110] [<ffff0000081767d8>] do_init_module+0x5c/0x1bc
[ 242.963714] [<ffff000008139650>] load_module+0x1c50/0x20f8
[ 242.969315] [<ffff000008139d78>] SyS_finit_module+0xa8/0xc0
[ 242.975003] [<ffff0000080838d8>] __sys_trace_return+0x0/0x4

Has anyone seen this problem?  Incidentally, a co-worker independently found the same problem.  It would be nice to know if I'm either mis-reading the instructions or the image has an error.

Thanks,

Glen

ラベル(2)
タグ(2)
0 件の賞賛
返信
4 返答(返信)

3,910件の閲覧回数
lingguan
Contributor II

Hi,

   I am seeing the same problem.  So I have to use 4.9.51 instead of 4.9.88?

0 件の賞賛
返信

3,911件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi GLENN

currently fully functional and tested is  Linux L4.9.51 for i.MX 8MQuad GA :

Demo

https://www.nxp.com/webapp/Download?colCode=L4.9.51_IMX8MQ_GA&appType=license&location=null&Parent_n... 

as stated in documentation (Release Notes) on i.MX software web page

i.MX Software|NXP 

According to attached Release Notes L4.9.88 has i.MX8M support in "Beta Quality".

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,911件の閲覧回数
ryanpabis
Contributor II

I am seeing the EXACT same thing!!!  Since 4.9.88 is a ga release it was my understanding it was safe to use.

root@imx8mqevk:~# [ 242.787553] INFO: task systemd-udevd:2850 blocked for more than 120 seconds.
[ 242.794685] Tainted: G O 4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d #1
[ 242.802443] "echo 0 > /proc/sys/kernel/hung_task_timeout_secs" disables this message.
[ 242.810431] systemd-udevd D 0 2850 1726 0x0000020d
[ 242.816113] Call trace:
[ 242.818609] [<ffff000008085e98>] __switch_to+0x90/0xc0
[ 242.823925] [<ffff000008c653f0>] __schedule+0x178/0x590
[ 242.829302] [<ffff000008c65844>] schedule+0x3c/0xa8
[ 242.834341] [<ffff000008c688e4>] schedule_timeout+0x174/0x248
[ 242.840242] [<ffff000008c67680>] __down+0x58/0x90
[ 242.845112] [<ffff000008102e74>] down+0x4c/0x68
[ 242.851364] [<ffff000000ec255c>] HIFExchangeBMIMsg+0x20c/0x330 [wlan]
[ 242.859362] [<ffff000000ec8ac4>] bmi_download_firmware+0x64/0x130 [wlan]
[ 242.867967] [<ffff000000e60f9c>] vos_open+0x174/0x6c0 [wlan]
[ 242.874797] [<ffff000000d1cca4>] hdd_wlan_startup+0x5ac/0x12e0 [wlan]
[ 242.882346] [<ffff000000ec6cc8>] hif_pci_probe+0x5f8/0x858 [wlan]
[ 242.888633] [<ffff000008486c4c>] pci_device_probe+0x9c/0x140
[ 242.894459] [<ffff000008649a40>] driver_probe_device+0x1d0/0x2c8
[ 242.900629] [<ffff000008649bf4>] __driver_attach+0xbc/0xc0
[ 242.906271] [<ffff000008647b34>] bus_for_each_dev+0x4c/0x98
[ 242.911993] [<ffff0000086493b8>] driver_attach+0x20/0x28
[ 242.917520] [<ffff000008648fa8>] bus_add_driver+0x1b8/0x228
[ 242.923245] [<ffff00000864a578>] driver_register+0x60/0xf8
[ 242.928975] [<ffff0000084857a8>] __pci_register_driver+0x38/0x40
[ 242.936369] [<ffff000000ec6630>] hif_register_driver+0x18/0x38 [wlan]
[ 242.944255] [<ffff000000d14d80>] hdd_hif_register_driver+0x30/0x78 [wlan]
[ 242.952412] [<ffff0000011790b4>] hdd_module_init+0xb4/0x1000 [wlan]
[ 242.958877] [<ffff000008083a50>] do_one_initcall+0x38/0x130
[ 242.964611] [<ffff0000081767d8>] do_init_module+0x5c/0x1bc
[ 242.970249] [<ffff000008139650>] load_module+0x1c50/0x20f8
[ 242.975884] [<ffff000008139d78>] SyS_finit_module+0xa8/0xc0
[ 242.981603] [<ffff0000080838d8>] __sys_trace_return+0x0/0x4

0 件の賞賛
返信

3,911件の閲覧回数
ryanpabis
Contributor II

One other thing I would like to mention now that I realize it's in beta is that sysVinit does not seem to work either.  If you comment out the systemd section in fsl-imx-preferred-env.inc the boot times are incredibly slow and you get a lot of udevd errors.

0 件の賞賛
返信