Kernel Panic error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kernel Panic error

8,592件の閲覧回数
arumugamramasam
Contributor II

Hi,

I am facing a kernel panic error when booting iMX25 PDK with SD Card. Need help to resolve this error. Screen shot is attached

Thanks,

Arumugam R

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

7,069件の閲覧回数
carlosorriento
Contributor II

I have exactly the same problem, very frustrating. I need to establish a working toolchain, or abandon this and find something that works.

I installed the Linux VM on a Windows system.  BTE: The system REALLY should ship with an errata sheet -- just getting thru the apt updates was annoying. But set that aside.

I ran the config, set in a few options, did a build, and made an SD card.  Kernel panic.

Examine the config about 12 times, same thing.

Okay, maybe I did something horribly wrong.  Build a pristine VM, run configure and accept the defaults.  Build a new image, copy to SD card.

Same crap.  Boot file is attached.

Any ideas where to go from here ? Or should I give up ?

0 件の賞賛
返信

7,069件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

I looked at your log, and it does seem to be a different issue as the one reported in this thread.

Your log does not show your complete kernel command line, but you are passing "gpmi" and trying to boot from SD card.

This is not correct as per the mx28evk Linux BSP User Guide document. You should pass "ssp1" instead.

Other than that, you are using a 2.6.31 kernel on mx28evk and I would strongly recommend to upgrade this kernel and the options are:

- 2.6.35 kernel from FSL + LTIB root file system

- 3.8 kernel from kernel.org + Yocto root file system

Both options work well.

By the way, Yocto generates an image that you can simply do a 'dd' into your SD card and you have a bootable system.

0 件の賞賛
返信

7,069件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

It seems you have a bad rootfs flashed into the SD card. For a quick test, you can try to booting via NFS.

7,069件の閲覧回数
LeonardoSandova
Specialist I

Could you share the full kernel log before the kernel panic?

7,069件の閲覧回数
arumugamramasam
Contributor II

Hi,

Please find below full log. Please let me know if you find anything wrong...

U-Boot 2009.08 (Jan 10 2013 - 17:01:27)

CPU:   Freescale i.MX25 at 398 MHz

mx25 cpu clock: 398MHz

ipg clock     : 66498560Hz

Board: i.MX25 MAX PDK (3DS)

I2C:   ready

DRAM:  64 MB

NAND:  Unrecognized NAND Flash device.

256 MiB

MMC:   FSL_ESDHC: 0

In:    serial

Out:   serial

Err:   serial

Net:   smc911x-0 [PRIME], FEC0

Hit any key to stop autoboot:  3     2     1     0

MMC read: dev # 0, block # 2048, count 4096 ... 4096 blocks read: OK

## Booting kernel from Legacy Image at 80800000 ...

   Image Name:   Linux-2.6.31-207-g7286c01

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    2026988 Bytes =  1.9 MB

   Load Address: 80008000

   Entry Point:  80008000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

Starting kernel ...

Uncompressing Linux.............................................................

................................................................................

.. done, booting the kernel.

Linux version 2.6.31-207-g7286c01 (arumugam@arumugam-laptop) (gcc version 4.1.2)

#2 PREEMPT Mon Feb 11 16:18:16 IST 2013

CPU: ARM926EJ-S [41069264] revision 4 (ARMv5TEJ), cr=00053177

CPU: VIVT data cache, VIVT instruction cache

Machine: Freescale MX25 3-Stack Board

Memory policy: ECC disabled, Data cache writeback

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 16256

Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p1 ip=none rootfsty

pe=ext2 init=/etc/inittab

PID hash table entries: 256 (order: 8, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory: 64MB = 64MB total

Memory: 60156KB available (3768K code, 454K data, 420K init, 0K highmem)

NR_IRQS:272

MXC IRQ initialized

Clock input source is 24000000

Console: colour dummy device 80x30

Calibrating delay loop... 199.06 BogoMIPS (lpj=995328)

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

regulator: core version 0.5

NET: Registered protocol family 16

AIPS1 VA base: 0xfc000000

CPU is i.MX25 Revision 1.0

MXC GPIO hardware

Using SDMA I.API

MXC DMA API initialized

bio: create slab <bio-0> at 0

SCSI subsystem initialized

CSPI: mxc_spi-0 probed

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

MXC I2C driver

regulator: REG1_BKLT: 4500 <--> 5500 mV

regulator: REG2_CPU: 2640 <--> 3877 mV

regulator: REG3_CORE: 1160 <--> 1703 mV

regulator: REG4_DDR: 1440 <--> 2115 mV

regulator: REG5_PERS: 2640 <--> 3877 mV

mc34704 0-0054: Loaded

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

Bus freq driver module loaded

Registering the CPLD Driver

3-Stack Debug board detected, rev = 0x3000300

usb: Host 2 host (serial) registered

usb: DR OTG registered

usb: DR host (utmi) registered

usb: DR gadget (utmi) registered

i.MXC CPU frequency driver

JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

msgmni has been set to 117

io scheduler noop registered

io scheduler anticipatory registered

io scheduler deadline registered

io scheduler cfq registered (default)

MXC Backlight Device mxc_lcdc_bl.0 Initialized.

Console: switching to colour frame buffer device 80x30

mxc_sdc_fb mxc_sdc_fb.0: fb0: DISP0 BG fb device registered successfully.

mxc_sdc_fb mxc_sdc_fb.0: fb1: DISP0 FG fb device registered successfully.

Serial: MXC Internal UART driver

mxcintuart.0: ttymxc0 at MMIO 0x43f90000 (irq = 45) is a Freescale i.MX

console [ttymxc0] enabled

mxcintuart.1: ttymxc1 at MMIO 0x43f94000 (irq = 32) is a Freescale i.MX

brd: module loaded

loop: module loaded

Freescale FlexCAN Driver

MXC MTD nand Driver 2.5

NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron NAND 256MiB 3,3V 8-bit

)

Unrecognized NAND Flash device.

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

MXC keypad loaded

input: mxckpd as /class/input/input0

IMXDI Realtime Clock Driver (RTC)

imxdi_rtc imxdi_rtc.0: rtc core: registered imxdi_rtc as rtc0

Linux video capture interface: v2.00

PMIC Character device: successfully loaded

i.MX ADC at 0x50030000 irq 46

mxsdhci: MXC Secure Digital Host Controller Interface driver

mxsdhci: MXC SDHCI Controller Driver.

mmc0: SDHCI detect irq 161 irq 9 INTERNAL DMA

usbcore: registered new interface driver usbhid

usbhid: v2.6:USB HID core driver

Advanced Linux Sound Architecture Driver Version 1.0.20.

regulator: Unable to get requested regulator: VDDD

sgtl5000-i2c 0-000a: SGTL5000 revision 17

No device for DAI imx-ssi-1-0

No device for DAI imx-ssi-1-1

No device for DAI imx-ssi-2-0

No device for DAI imx-ssi-2-1

DMA Sound Buffers Allocated:UseIram=1 buf->addr=78001000 buf->area=c4880000 size

=65536

DMA Sound Buffers Allocated:UseIram=1 buf->addr=83a90000 buf->area=fdf2d000 size

=65536

asoc: SGTL5000 <-> imx-ssi-1-0 mapping ok

mmc0: new high speed SDHC card at address e624

mmcblk0: mmc0:e624 SU04G 3.69 GiB

mmcblk0: p1

ALSA device list:

  #0: imx-3stack (SGTL5000)

oprofile: using timer interrupt.

TCP cubic registered

NET: Registered protocol family 17

can: controller area network core (rev 20090105 abi 8)

NET: Registered protocol family 29

can: raw protocol (rev 20090105)

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

smsc911x: Driver version 2008-10-21.

smsc911x-mdio: probed

eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1)

net eth0: MAC Address: 00:04:9f:01:d6:c3

Static Power Management for Freescale i.MX25

regulator_init_complete: incomplete constraints, leaving REG5_PERS on

regulator_init_complete: incomplete constraints, leaving REG1_BKLT on

input: imx_adc_ts as /class/input/input1

i.MX ADC input touchscreen loaded.

imxdi_rtc imxdi_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)

EXT2-fs warning: mounting unchecked fs, running e2fsck is recommended

VFS: Mounted root (ext2 filesystem) on device 179:1.

Freeing init memory: 420K

Failed to execute /etc/inittab.  Attempting defaults...

Kernel panic - not syncing: No init found.  Try passing init= option to kernel.

Thanks,

Arumugam R

0 件の賞賛
返信

7,069件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

It's preferred to use ext3 instead of ext2.

Try the command line below as per mx25 Linux BSP User guide document:

noinitrd console=ttymxc0 root=/dev/mmcblk0p1 rootfstype=ext3 rw ip=dhcp


0 件の賞賛
返信