Kernel Menuconfig reset problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kernel Menuconfig reset problem

ソリューションへジャンプ
4,393件の閲覧回数
brianhuang
Contributor II

Hi

I follow below steps building fsl-yocto-L4.1.15_1.1.0-ga for our custom imx6q board

1."MACHINE=imx6qsabresd source fsl-setup-release.sh -b build -e x11"

2."bitbake fsl-image-qt5"

3.When the building tasks is all done,I merge my driver to linux-imx and use "bitbake -c menuconfig linux-imx" for custom .config file.

4.merge our test application to imx-test

5."bitbake -c compile linux-imx -f"

6."bitbake -c compile imx-test -f"

After step 6. ,I found my .config file is reset to default.

How can I stop this reset operation? Which file do I need modify

Thank you.

Brian Huang

ラベル(3)
タグ(1)
1 解決策
3,761件の閲覧回数
brianhuang
Contributor II

Hi Yuri

Sorry for reply lately.

Thanks for your answer.

I found the solution in yocto document

Yocto Project Development Manual

5.9.2. Creating a  defconfig File and 5.9.3. Creating Configuration Fragments is very useful for my problem

元の投稿で解決策を見る

2 返答(返信)
3,760件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Hope the following helps.

How to modify yocto jethro and rebuild

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,762件の閲覧回数
brianhuang
Contributor II

Hi Yuri

Sorry for reply lately.

Thanks for your answer.

I found the solution in yocto document

Yocto Project Development Manual

5.9.2. Creating a  defconfig File and 5.9.3. Creating Configuration Fragments is very useful for my problem