Kernel Drivers/Modules from gki.fragment Not Loaded After OTA Update in i.MX8MQ(Android14_2.0.0)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel Drivers/Modules from gki.fragment Not Loaded After OTA Update in i.MX8MQ(Android14_2.0.0)

734 Views
Maruti
Contributor III

Dear Team,

We are working with Android 14_2.0.0 on a custom board based on the i.MX8MQ platform. We are including our drivers and kernel modules using a gki.fragment configuration.

Issue Description:

  • Before OTA Update:

    • The board boots from the boot_a slot.

    • All drivers and kernel modules defined in gki.fragment are correctly loaded at boot.

    • Functionality dependent on these modules works as expected.

  • After OTA Update:

    • The board boots successfully from the boot_b slot.

    • However, none of the drivers or kernel modules from gki.fragment are loaded.

    • This causes critical features relying on those modules to break.

Additional Information:

  • GKI Kernel Version: 6.6.30

  • Kernel Version Before OTA: 6.6.30-4k-g83331275a61f-dirty

  • Kernel Version After OTA: 6.6.30-android15-8-g63f82df87330-ab12046046-4k

Could you please help us identify what might be missing or misconfigured? We need a solution to ensure that the gki.fragment modules load correctly after an OTA update.

Regards,
Maruti Naik

0 Kudos
Reply
3 Replies

729 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

 

please check 
1.  device/nxp/imx8q/mek_8q/SharedBoardConfig.mk  
please make sure all the modules you added  are listed in this file
 
 
2. This file (SharedBoardConfig.mk)
divides the storage locations of the kernel modules into two parts :  one is inside the ramdisk.  and the other is in the vendor_dlkm partition.
 
You can check the directories  $OUT/vendor_ramdisk/lib/modules/ and $OUT/vendor_dlkm/lib/modules/ to see if the files you need are there. 
 
Regards
Daniel
0 Kudos
Reply

585 Views
Maruti
Contributor III

Hi Daniel,

Yes, I have checked — the modules are present in the vendor_dlkm/lib/modules directory.
With normal binary flashing, all the modules load without any issues.
This problem occurs only after the OTA update.

Regards,
Maruti Naik

Tags (2)
0 Kudos
Reply

520 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @Maruti 

please share the detailed steps so I can reproduce this issue on my side.

 

Regards

Daniel

0 Kudos
Reply