Kernel Crash while updating board using Swupdate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel Crash while updating board using Swupdate

2,105 Views
Aakash_Sharma
Contributor II

Hi,

We are using IMX8MQ EVK and trying to do Firmware Upgrade using Swupdate utility (version 2020.04) . Board is running on yocto Linux 5.4-zeus distribution and while upgrading the board, swupdate flash progress reaches 95% and then generates kernel crash. Below are the different kernel crash attached logs we are getting with each time we execute the firmware upgrade.

 

Also, we have seen that our RAM is 3GB and it's working as expected and also there's no full memory utilization.

So, please review attached logs and provide the support for the same.

Thanks,

Aakash

 

0 Kudos
Reply
0 Replies