Not able to mount android 11 partitions imx computed Dev board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to mount android 11 partitions imx computed Dev board

3,192件の閲覧回数
swapnilpendhare
Contributor III

Hi, 
I am trying to boot Android 11 Build on iMX8MP compulab EVK board, I am able to boot Android OS from SD card, 

But not able to get partition mounted in 10 Seconds, I have worked on all the required drivers and Power supply related issue. 

I am not sure what is the problem right now. 
1. Is 10 second time not enough for mounting. Or

2. I am missing something in DTS or Driver side. 

Please help me on this. 


=========================================================================

U-Boot SPL 2021.04-00001-g302084ead7-dirty (Mar 27 2022 - 14:18:05 +0530)
DDRINFO: Cfg attempt: [ 3/4 ]
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
DDRINFO(M): mr5-8 [ 0xff000010 ]
DDRINFO(T): mr5-8 [ 0xff000010 ]
DDRINFO(E): mr5-8 [ 0xff000010 ], read back
spl_dram_init Continue w/out reset ...
Normal Boot
WDT: Not starting
Trying to boot from BOOTROM
image offset 0x8000, pagesize 0x200, ivt offset 0x0
Failed to find node!, err: -1!
Failed to find node!, err: -1!
NOTICE: BL31: v2.4(release):android-11.0.0_2.6.0-0-g2ff011d64
NOTICE: BL31: Built : 14:18:58, Mar 27 2022


U-Boot 2021.04-00001-g302084ead7-dirty (Mar 27 2022 - 14:18:05 +0530)

CPU: i.MX8MP[8] rev1.1 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 59C
Reset cause: POR
Model: CompuLab UCM-iMX8M-Plus
DRAM: 4 GiB
WDT: Started with servicing (60s timeout)
MMC: FSL_SDHC: 1, FSL_SDHC: 2
[*]-Video Link 0 (720 x 1280)
[0] lcd-controller@32e80000, video
[1] mipi_dsi@32e60000, video_bridge
[2] ili9881c_panel, panel
In: serial
Out: serial
Err: serial

BuildInfo:
- ATF 2ff011d

flash target is MMC:1
Net: eth1: ethernet@30bf0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
In boota get fastboot lock status error. Set lock status
Magic is incorrect.
Error validating A/B metadata from disk. Resetting and writing new A/B metadata to disk.
Writing A/B metadata to disk.
verify OK, boot 'boot_a'
Kernel load addr 0x40480000 size 53319 KiB
kernel @ 40480000 (52035584)
ramdisk @ 44680000 (8509180)
fdt @ 437a0400 (64433)
Moving Image from 0x40480000 to 0x40600000, end=437a0000
## Flattened Device Tree blob at 437a0400
Booting using the fdt blob at 0x437a0400
Using Device Tree in place at 00000000437a0400, end 00000000437b2fb0

Starting kernel ...

[ 0.000000][ T0] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000][ T0] Linux version 5.10.72-00001-gcb6f328b5e81-dirty (swapnil@AGLPUN-D0322U) (Android (7284624, based on r416183b) clang version 12.0.5 (https://android.googlesource.com/toolchain/llvm-project c935d99d7cf2016289302412d708641d52d2f7ee), LLD 12.0.5 (/buildbot/src/android/llvm-toolchain/out/llvm-project/lld c935d99d7cf2016289302412d708641d52d2f7ee)) #8 SMP PREEMPT Mon Mar 28 00:46:30 IST 2022
[ 0.000000][ T0] Machine model: CompuLab UCM-iMX8M-Plus
[ 0.000000][ T0] Stack Depot is disabled
[ 0.000000][ T0] earlycon: ec_imx6q0 at MMIO 0x0000000030890000 (options '115200')
[ 0.000000][ T0] printk: bootconsole [ec_imx6q0] enabled
[ 0.000000][ T0] efi: UEFI not found.
[ 0.000000][ T0] Reserved memory: bypass linux,cma node, using cmdline CMA params instead
[ 0.000000][ T0] OF: reserved mem: node linux,cma compatible matching fail
[ 0.000000][ T0] Reserved memory: created DMA memory pool at 0x0000000094300000, size 1 MiB
[ 0.000000][ T0] OF: reserved mem: initialized node vdev0buffer@94300000, compatible id shared-dma-pool
[ 0.000000][ T0] NUMA: No NUMA configuration found
[ 0.000000][ T0] NUMA: Faking a node at [mem 0x0000000040000000-0x000000013fffffff]
[ 0.000000][ T0] NUMA: NODE_DATA [mem 0x13f848680-0x13f84afff]
[ 0.000000][ T0] Zone ranges:
[ 0.000000][ T0] DMA [mem 0x0000000040000000-0x00000000ffffffff]
[ 0.000000][ T0] DMA32 empty
[ 0.000000][ T0] Normal [mem 0x0000000100000000-0x000000013fffffff]
[ 0.000000][ T0] Movable zone start for each node
[ 0.000000][ T0] Early memory node ranges
[ 0.000000][ T0] node 0: [mem 0x0000000040000000-0x00000000557fffff]
[ 0.000000][ T0] node 0: [mem 0x0000000055800000-0x0000000055ffffff]
[ 0.000000][ T0] node 0: [mem 0x0000000056000000-0x00000000823fffff]
[ 0.000000][ T0] node 0: [mem 0x0000000082400000-0x00000000943fffff]
[ 0.000000][ T0] node 0: [mem 0x0000000094400000-0x00000000944fffff]
[ 0.000000][ T0] node 0: [mem 0x0000000094500000-0x000000009450ffff]
[ 0.000000][ T0] node 0: [mem 0x0000000094510000-0x000000013fffffff]
[ 0.000000][ T0] Initmem setup node 0 [mem 0x0000000040000000-0x000000013fffffff]
[ 0.000000][ T0] cma: Reserved 960 MiB at 0x00000000a4000000
[ 0.000000][ T0] psci: probing for conduit method from DT.
[ 0.000000][ T0] psci: PSCIv1.1 detected in firmware.
[ 0.000000][ T0] psci: Using standard PSCI v0.2 function IDs
[ 0.000000][ T0] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000][ T0] psci: SMC Calling Convention v1.2
[ 0.000000][ T0] percpu: Embedded 33 pages/cpu s97432 r8192 d29544 u135168
[ 0.000000][ T0] Detected VIPT I-cache on CPU0
[ 0.000000][ T0] CPU features: detected: ARM erratum 845719
[ 0.000000][ T0] CPU features: detected: GIC system register CPU interface
[ 0.000000][ T0] Built 1 zonelists, mobility grouping on. Total pages: 1032192
[ 0.000000][ T0] Policy zone: Normal
[ 0.000000][ T0] Kernel command line: stack_depot_disable=on=kasan.stacktrace=off console=ttymxc1,115200 earlycon=ec_imx6q,0x30890000,115200 console=tty0 init=/init androidboot.console=ttymxc1 androidboot.hardware=nxp firmware_class.path=/vendor/firmware loop.max_part=7 transparent_hugepage=never swiotlb=65536 androidboot.lcd_density=240 androidboot.primary_display=imx-drm cma=960M@0x400M-0x1000M androidboot.vendor.sysrq=1 buildvariant=userdebug androidboot.serialno=062040000882277a androidboot.btmacaddr=06:20:40:00:08:82 androidboot.soc_type=imx8mp androidboot.boot_device_root=mmcblk1 androidboot.boottime=1BLL:0,1BLE:8211,KL:0,KD:0,AVB:4436,ODT:0,SW:0 androidboot.bootreason=cold,powerkey androidboot.dtbo_idx=0 androidboot.keystore=software androidboot.verifiedbootstate=green androidboot.flash.locked=1 androidboot.slot_suffix=_a androidboot.vbmeta.device=PARTUUID=9745acf3-fa57-452f-b47c-ee99c34a59d5 androidboot.vbmeta.avb_version=1.1 androidboot.vbmeta.device_state=locked and
[ 0.000000][ T0] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000][ T0] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000][ T0] mem auto-init: stack:all(zero), heap alloc:on, heap free:off
[ 0.000000][ T0] software IO TLB: mapped [mem 0x00000000f7fff000-0x00000000fffff000] (128MB)
[ 0.000000][ T0] Memory: 2373136K/4194304K available (30848K kernel code, 2306K rwdata, 12980K rodata, 3456K init, 1037K bss, 838128K reserved, 983040K cma-reserved)
[ 0.000000][ T0] random: get_random_u64 called from kmem_cache_open+0x34/0x498 with crng_init=0
[ 0.000000][ T0] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000][ T0] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000][ T0] rcu: RCU event tracing is enabled.
[ 0.000000][ T0] rcu: RCU dyntick-idle grace-period acceleration is enabled.
[ 0.000000][ T0] rcu: RCU restricting CPUs from NR_CPUS=32 to nr_cpu_ids=4.
[ 0.000000][ T0] Trampoline variant of Tasks RCU enabled.
[ 0.000000][ T0] Tracing variant of Tasks RCU enabled.
[ 0.000000][ T0] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000][ T0] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000][ T0] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000][ T0] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000][ T0] GICv3: 160 SPIs implemented
[ 0.000000][ T0] GICv3: 0 Extended SPIs implemented
[ 0.000000][ T0] GICv3: Distributor has no Range Selector support
[ 0.000000][ T0] GICv3: 16 PPIs implemented
[ 0.000000][ T0] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000][ T0] ITS: No ITS available, not enabling LPIs
[ 0.000000][ T0] rcu: Offload RCU callbacks from CPUs: (none).
[ 0.000000][ T0] kfence: initialized - using 524288 bytes for 63 objects at 0x(____ptrval____)-0x(____ptrval____)
[ 0.000000][ T0] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000][ T0] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000003][ T0] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.009600][ T0] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.019783][ T0] pid_max: default: 32768 minimum: 301
[ 0.025224][ T0] LSM: Security Framework initializing
[ 0.030505][ T0] SELinux: Initializing.
[ 0.034789][ T0] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.042805][ T0] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.053182][ T1] rcu: Hierarchical SRCU implementation.
[ 0.057612][ T1] EFI services will not be available.
[ 0.062380][ T1] smp: Bringing up secondary CPUs ...
[ 0.067950][ T0] Detected VIPT I-cache on CPU1
[ 0.067976][ T0] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.068013][ T0] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.068576][ T0] Detected VIPT I-cache on CPU2
[ 0.068593][ T0] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.068615][ T0] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.069179][ T0] Detected VIPT I-cache on CPU3
[ 0.069194][ T0] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.069216][ T0] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.069292][ T1] smp: Brought up 1 node, 4 CPUs
[ 0.131012][ T1] SMP: Total of 4 processors activated.
[ 0.136420][ T1] CPU features: detected: 32-bit EL0 Support
[ 0.142304][ T1] CPU features: detected: CRC32 instructions
[ 0.148151][ T1] CPU features: detected: 32-bit EL1 Support
[ 0.154070][ T1] CPU features: emulated: Privileged Access Never (PAN) using TTBR0_EL1 switching
[ 0.193531][ T1] CPU: All CPU(s) started at EL2
[ 0.195518][ T14] alternatives: patching kernel code
[ 0.204902][ T1] devtmpfs: initialized
[ 0.218322][ T1] Registered cp15_barrier emulation handler
[ 0.221260][ T1] Registered setend emulation handler
[ 0.226499][ T1] KASLR disabled due to lack of seed
[ 0.231819][ T1] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.242176][ T1] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.307709][ T1] pinctrl core: initialized pinctrl subsystem
[ 0.311507][ T1] DMI not present or invalid.
[ 0.315747][ T1] NET: Registered protocol family 16
[ 0.333235][ T1] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[ 0.338437][ T1] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.347056][ T1] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.355470][ T1] audit: initializing netlink subsys (disabled)
[ 0.361691][ T37] audit: type=2000 audit(0.276:1): state=initialized audit_enabled=0 res=1
[ 0.362216][ T1] thermal_sys: Registered thermal governor 'step_wise'
[ 0.369941][ T1] thermal_sys: Registered thermal governor 'user_space'
[ 0.376671][ T1] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.383851][ T1] cpuidle: using governor menu
[ 0.395879][ T1] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.403009][ T1] ASID allocator initialised with 65536 entries
[ 0.409332][ T1] Serial: AMBA PL011 UART driver
[ 0.413926][ T1] imx mu driver is registered.
[ 0.418513][ T1] imx rpmsg driver is registered.
[ 0.424219][ T1] printk: console [ramoops-1] enabled
[ 0.428858][ T1] pstore: Registered ramoops as persistent store backend
[ 0.435566][ T1] ramoops: using 0x100000@0x94400000, ecc: 0
[ 0.453937][ T1] imx8mp-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver
[ 0.502721][ T1] ACPI: Interpreter disabled.
[ 0.505536][ T1] iommu: Default domain type: Translated
[ 0.510590][ T1] SCSI subsystem initialized
[ 0.514871][ T1] usbcore: registered new interface driver usbfs
[ 0.520734][ T1] usbcore: registered new interface driver hub
[ 0.526760][ T1] usbcore: registered new device driver usb
[ 0.533585][ T1] mc: Linux media interface: v0.10
[ 0.537523][ T1] videodev: Linux video capture interface: v2.00
[ 0.543768][ T1] pps_core: LinuxPPS API ver. 1 registered
[ 0.549395][ T1] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.559294][ T1] PTP clock support registered
[ 0.564086][ T1] EDAC MC: Ver: 3.0.0
[ 0.569118][ T1] Advanced Linux Sound Architecture Driver Initialized.
[ 0.575251][ T1] nfc: nfc_init: NFC Core ver 0.1
[ 0.579537][ T1] NET: Registered protocol family 39
[ 0.585934][ T1] clocksource: Switched to clocksource arch_sys_counter
[ 0.672065][ T1] VFS: Disk quotas dquot_6.6.0
[ 0.673895][ T1] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.681566][ T1] pnp: PnP ACPI: disabled
[ 0.687370][ T1] NET: Registered protocol family 2
[ 0.690893][ T1] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.700742][ T1] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[ 0.708289][ T1] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.717083][ T1] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
[ 0.725323][ T1] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.732280][ T1] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.739654][ T1] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.747625][ T1] NET: Registered protocol family 1
[ 0.752533][ T1] NET: Registered protocol family 44
[ 0.757898][ T1] Trying to unpack rootfs image as initramfs...
[ 1.104347][ T1] Freeing initrd memory: 8308K
[ 1.107119][ T1] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 1.115284][ T1] kvm [1]: IPA Size Limit: 40 bits
[ 1.122645][ T1] kvm [1]: GICv3: no GICV resource entry
[ 1.125291][ T1] kvm [1]: disabling GICv2 emulation
[ 1.130473][ T1] kvm [1]: GIC system register CPU interface enabled
[ 1.137118][ T1] kvm [1]: vgic interrupt IRQ9
[ 1.141808][ T1] kvm [1]: Hyp mode initialized successfully
[ 1.151011][ T1] Initialise system trusted keyrings
[ 1.153508][ T1] workingset: timestamp_bits=42 max_order=20 bucket_order=0
[ 1.169287][ T1] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 1.173301][ T1] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 1.180433][ T1] fuse: init (API version 7.32)
[ 1.226415][ T1] Key type asymmetric registered
[ 1.228380][ T1] Asymmetric key parser 'x509' registered
[ 1.234023][ T1] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 235)
[ 1.242140][ T1] io scheduler mq-deadline registered
[ 1.247376][ T1] io scheduler kyber registered
[ 1.252250][ T1] io scheduler bfq registered
[ 1.259855][ T1] pwm-backlight dsi_backlight: supply power not found, using dummy regulator
[ 1.266106][ T1] pwm-backlight lvds_backlight: supply power not found, using dummy regulator
[ 1.280621][ T1] clk: failed to reparent gic to sys_pll2_500m: -16
[ 1.289374][ T1] mxs-dma 33000000.dma-apbh: initialized
[ 1.292849][ T1] SoC: i.MX8MP revision 1.1
[ 1.296907][ T1] Bus freq driver module loaded
[ 1.303046][ T1] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[ 1.310789][ T1] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 36, base_baud = 1500000) is a IMX
[ 0.000000][ T0] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000][ T0] Linux version 5.10.72-00001-gcb6f328b5e81-dirty (swapnil@AGLPUN-D0322U) (Android (7284624, based on r416183b) clang version 12.0.5 (https://android.googlesource.com/toolchain/llvm-project c935d99d7cf2016289302412d708641d52d2f7ee), LLD 12.0.5 (/buildbot/src/android/llvm-toolchain/out/llvm-project/lld c935d99d7cf2016289302412d708641d52d2f7ee)) #8 SMP PREEMPT Mon Mar 28 00:46:30 IST 2022
[ 0.000000][ T0] Machine model: CompuLab UCM-iMX8M-Plus
[ 0.000000][ T0] Stack Depot is disabled
[ 0.000000][ T0] earlycon: ec_imx6q0 at MMIO 0x0000000030890000 (options '115200')
[ 0.000000][ T0] printk: bootconsole [ec_imx6q0] enabled
[ 0.000000][ T0] efi: UEFI not found.
[ 0.000000][ T0] Reserved memory: bypass linux,cma node, using cmdline CMA params instead
[ 0.000000][ T0] OF: reserved mem: node linux,cma compatible matching fail
[ 0.000000][ T0] Reserved memory: created DMA memory pool at 0x0000000094300000, size 1 MiB
[ 0.000000][ T0] OF: reserved mem: initialized node vdev0buffer@94300000, compatible id shared-dma-pool
[ 0.000000][ T0] NUMA: No NUMA configuration found
[ 0.000000][ T0] NUMA: Faking a node at [mem 0x0000000040000000-0x000000013fffffff]
[ 0.000000][ T0] NUMA: NODE_DATA [mem 0x13f848680-0x13f84afff]
[ 0.000000][ T0] Zone ranges:
[ 0.000000][ T0] DMA [mem 0x0000000040000000-0x00000000ffffffff]
[ 0.000000][ T0] DMA32 empty
[ 0.000000][ T0] Normal [mem 0x0000000100000000-0x000000013fffffff]
[ 0.000000][ T0] Movable zone start for each node
[ 0.000000][ T0] Early memory node ranges
[ 0.000000][ T0] node 0: [mem 0x0000000040000000-0x00000000557fffff]
[ 0.000000][ T0] node 0: [mem 0x0000000055800000-0x0000000055ffffff]
[ 0.000000][ T0] node 0: [mem 0x0000000056000000-0x00000000823fffff]
[ 0.000000][ T0] node 0: [mem 0x0000000082400000-0x00000000943fffff]
[ 0.000000][ T0] node 0: [mem 0x0000000094400000-0x00000000944fffff]
[ 0.000000][ T0] node 0: [mem 0x0000000094500000-0x000000009450ffff]
[ 0.000000][ T0] node 0: [mem 0x0000000094510000-0x000000013fffffff]
[ 0.000000][ T0] Initmem setup node 0 [mem 0x0000000040000000-0x000000013fffffff]
[ 0.000000][ T0] cma: Reserved 960 MiB at 0x00000000a4000000
[ 0.000000][ T0] psci: probing for conduit method from DT.
[ 0.000000][ T0] psci: PSCIv1.1 detected in firmware.
[ 0.000000][ T0] psci: Using standard PSCI v0.2 function IDs
[ 0.000000][ T0] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000][ T0] psci: SMC Calling Convention v1.2
[ 0.000000][ T0] percpu: Embedded 33 pages/cpu s97432 r8192 d29544 u135168
[ 0.000000][ T0] Detected VIPT I-cache on CPU0
[ 0.000000][ T0] CPU features: detected: ARM erratum 845719
[ 0.000000][ T0] CPU features: detected: GIC system register CPU interface
[ 0.000000][ T0] Built 1 zonelists, mobility grouping on. Total pages: 1032192
[ 0.000000][ T0] Policy zone: Normal
[ 0.000000][ T0] Kernel command line:
stack_depot_disable=on=kasan.stacktrace=off
console=ttymxc1,115200
earlycon=ec_imx6q,0x30890000,115200
console=tty0
init=/init
androidboot.console=ttymxc1
androidboot.hardware=nxp
firmware_class.path=/vendor/firmware
loop.max_part=7
transparent_hugepage=never
swiotlb=65536 androidboot.lcd_density=240
androidboot.primary_display=imx-drm
cma=960M@0x400M-0x1000M
androidboot.vendor.sysrq=1
buildvariant=userdebug
androidboot.serialno=062040000882277a androidboot.btmacaddr=06:20:40:00:08:82
androidboot.soc_type=imx8mp
androidboot.boot_device_root=mmcblk1
androidboot.boottime=1BLL:0,1BLE:8211,KL:0,KD:0,AVB:4436,ODT:0,SW:0 androidboot.bootreason=cold,powerkey
androidboot.dtbo_idx=0
androidboot.keystore=software
androidboot.verifiedbootstate=green androidboot.flash.locked=1
androidboot.slot_suffix=_a androidboot.vbmeta.device=PARTUUID=9745acf3-fa57-452f-b47c-ee99c34a59d5
androidboot.vbmeta.avb_version=1.1
androidboot.vbmeta.device_state=locked and

[ 0.000000][ T0] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000][ T0] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000][ T0] mem auto-init: stack:all(zero), heap alloc:on, heap free:off
[ 0.000000][ T0] software IO TLB: mapped [mem 0x00000000f7fff000-0x00000000fffff000] (128MB)
[ 0.000000][ T0] Memory: 2373136K/4194304K available (30848K kernel code, 2306K rwdata, 12980K rodata, 3456K init, 1037K bss, 838128K reserved, 983040K cma-reserved)
[ 0.000000][ T0] random: get_random_u64 called from kmem_cache_open+0x34/0x498 with crng_init=0
[ 0.000000][ T0] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000][ T0] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000][ T0] rcu: RCU event tracing is enabled.
[ 0.000000][ T0] rcu: RCU dyntick-idle grace-period acceleration is enabled.
[ 0.000000][ T0] rcu: RCU restricting CPUs from NR_CPUS=32 to nr_cpu_ids=4.
[ 0.000000][ T0] Trampoline variant of Tasks RCU enabled.
[ 0.000000][ T0] Tracing variant of Tasks RCU enabled.
[ 0.000000][ T0] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000][ T0] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000][ T0] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000][ T0] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000][ T0] GICv3: 160 SPIs implemented
[ 0.000000][ T0] GICv3: 0 Extended SPIs implemented
[ 0.000000][ T0] GICv3: Distributor has no Range Selector support
[ 0.000000][ T0] GICv3: 16 PPIs implemented
[ 0.000000][ T0] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000][ T0] ITS: No ITS available, not enabling LPIs
[ 0.000000][ T0] rcu: Offload RCU callbacks from CPUs: (none).
[ 0.000000][ T0] kfence: initialized - using 524288 bytes for 63 objects at 0x(____ptrval____)-0x(____ptrval____)
[ 0.000000][ T0] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000][ T0] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000003][ T0] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.009600][ T0] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.019783][ T0] pid_max: default: 32768 minimum: 301
[ 0.025224][ T0] LSM: Security Framework initializing
[ 0.030505][ T0] SELinux: Initializing.
[ 0.034789][ T0] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.042805][ T0] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.053182][ T1] rcu: Hierarchical SRCU implementation.
[ 0.057612][ T1] EFI services will not be available.
[ 0.062380][ T1] smp: Bringing up secondary CPUs ...
[ 0.067950][ T0] Detected VIPT I-cache on CPU1
[ 0.067976][ T0] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.068013][ T0] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.068576][ T0] Detected VIPT I-cache on CPU2
[ 0.068593][ T0] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.068615][ T0] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.069179][ T0] Detected VIPT I-cache on CPU3
[ 0.069194][ T0] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.069216][ T0] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.069292][ T1] smp: Brought up 1 node, 4 CPUs
[ 0.131012][ T1] SMP: Total of 4 processors activated.
[ 0.136420][ T1] CPU features: detected: 32-bit EL0 Support
[ 0.142304][ T1] CPU features: detected: CRC32 instructions
[ 0.148151][ T1] CPU features: detected: 32-bit EL1 Support
[ 0.154070][ T1] CPU features: emulated: Privileged Access Never (PAN) using TTBR0_EL1 switching
[ 0.193531][ T1] CPU: All CPU(s) started at EL2
[ 0.195518][ T14] alternatives: patching kernel code
[ 0.204902][ T1] devtmpfs: initialized
[ 0.218322][ T1] Registered cp15_barrier emulation handler
[ 0.221260][ T1] Registered setend emulation handler
[ 0.226499][ T1] KASLR disabled due to lack of seed
[ 0.231819][ T1] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.242176][ T1] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.307709][ T1] pinctrl core: initialized pinctrl subsystem
[ 0.311507][ T1] DMI not present or invalid.
[ 0.315747][ T1] NET: Registered protocol family 16
[ 0.333235][ T1] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[ 0.338437][ T1] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.347056][ T1] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.355470][ T1] audit: initializing netlink subsys (disabled)
[ 0.361691][ T37] audit: type=2000 audit(0.276:1): state=initialized audit_enabled=0 res=1
[ 0.362216][ T1] thermal_sys: Registered thermal governor 'step_wise'
[ 0.369941][ T1] thermal_sys: Registered thermal governor 'user_space'
[ 0.376671][ T1] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.383851][ T1] cpuidle: using governor menu
[ 0.395879][ T1] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.403009][ T1] ASID allocator initialised with 65536 entries
[ 0.409332][ T1] Serial: AMBA PL011 UART driver
[ 0.413926][ T1] imx mu driver is registered.
[ 0.418513][ T1] imx rpmsg driver is registered.
[ 0.424219][ T1] printk: console [ramoops-1] enabled
[ 0.428858][ T1] pstore: Registered ramoops as persistent store backend
[ 0.435566][ T1] ramoops: using 0x100000@0x94400000, ecc: 0
[ 0.453937][ T1] imx8mp-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver
[ 0.502721][ T1] ACPI: Interpreter disabled.
[ 0.505536][ T1] iommu: Default domain type: Translated
[ 0.510590][ T1] SCSI subsystem initialized
[ 0.514871][ T1] usbcore: registered new interface driver usbfs
[ 0.520734][ T1] usbcore: registered new interface driver hub
[ 0.526760][ T1] usbcore: registered new device driver usb
[ 0.533585][ T1] mc: Linux media interface: v0.10
[ 0.537523][ T1] videodev: Linux video capture interface: v2.00
[ 0.543768][ T1] pps_core: LinuxPPS API ver. 1 registered
[ 0.549395][ T1] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.559294][ T1] PTP clock support registered
[ 0.564086][ T1] EDAC MC: Ver: 3.0.0
[ 0.569118][ T1] Advanced Linux Sound Architecture Driver Initialized.
[ 0.575251][ T1] nfc: nfc_init: NFC Core ver 0.1
[ 0.579537][ T1] NET: Registered protocol family 39
[ 0.585934][ T1] clocksource: Switched to clocksource arch_sys_counter
[ 0.672065][ T1] VFS: Disk quotas dquot_6.6.0
[ 0.673895][ T1] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.681566][ T1] pnp: PnP ACPI: disabled
[ 0.687370][ T1] NET: Registered protocol family 2
[ 0.690893][ T1] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.700742][ T1] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[ 0.708289][ T1] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.717083][ T1] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
[ 0.725323][ T1] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.732280][ T1] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.739654][ T1] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.747625][ T1] NET: Registered protocol family 1
[ 0.752533][ T1] NET: Registered protocol family 44
[ 0.757898][ T1] Trying to unpack rootfs image as initramfs...
[ 1.104347][ T1] Freeing initrd memory: 8308K
[ 1.107119][ T1] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 1.115284][ T1] kvm [1]: IPA Size Limit: 40 bits
[ 1.122645][ T1] kvm [1]: GICv3: no GICV resource entry
[ 1.125291][ T1] kvm [1]: disabling GICv2 emulation
[ 1.130473][ T1] kvm [1]: GIC system register CPU interface enabled
[ 1.137118][ T1] kvm [1]: vgic interrupt IRQ9
[ 1.141808][ T1] kvm [1]: Hyp mode initialized successfully
[ 1.151011][ T1] Initialise system trusted keyrings
[ 1.153508][ T1] workingset: timestamp_bits=42 max_order=20 bucket_order=0
[ 1.169287][ T1] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 1.173301][ T1] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 1.180433][ T1] fuse: init (API version 7.32)
[ 1.226415][ T1] Key type asymmetric registered
[ 1.228380][ T1] Asymmetric key parser 'x509' registered
[ 1.234023][ T1] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 235)
[ 1.242140][ T1] io scheduler mq-deadline registered
[ 1.247376][ T1] io scheduler kyber registered
[ 1.252250][ T1] io scheduler bfq registered
[ 1.259855][ T1] pwm-backlight dsi_backlight: supply power not found, using dummy regulator
[ 1.266106][ T1] pwm-backlight lvds_backlight: supply power not found, using dummy regulator
[ 1.280621][ T1] clk: failed to reparent gic to sys_pll2_500m: -16
[ 1.289374][ T1] mxs-dma 33000000.dma-apbh: initialized
[ 1.292849][ T1] SoC: i.MX8MP revision 1.1
[ 1.296907][ T1] Bus freq driver module loaded
[ 1.303046][ T1] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[ 1.310789][ T1] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 36, base_baud = 1500000) is a IMX
[ 2.577760][ T1] printk: console [ttymxc1] enabled
[ 2.577760][ T1] printk: console [ttymxc1] enabled
[ 2.602360][ T1] brd: module loaded
[ 2.602360][ T1] brd: module loaded
[ 2.620801][ T1] loop: module loaded
[ 2.620801][ T1] loop: module loaded
[ 2.628862][ T1] zram: Added device: zram0
[ 2.628862][ T1] zram: Added device: zram0
[ 2.638657][ T7] nd_pmem namespace0.0: unable to guarantee persistence of writes
[ 2.638657][ T7] nd_pmem namespace0.0: unable to guarantee persistence of writes
[ 2.640498][ T1] imx ahci driver is registered.
[ 2.640498][ T1] imx ahci driver is registered.
[ 2.665979][ T1] wireguard: WireGuard 1.0.0 loaded. See www.wireguard.com for information.
[ 2.665979][ T1] wireguard: WireGuard 1.0.0 loaded. See www.wireguard.com for information.
[ 2.683039][ T1] wireguard: Copyright (C) 2015-2019 Jason A. Donenfeld <Jason@zx2c4.com>. All Rights Reserved.
[ 2.683039][ T1] wireguard: Copyright (C) 2015-2019 Jason A. Donenfeld <Jason@zx2c4.com>. All Rights Reserved.
[ 2.704830][ T1] libphy: Fixed MDIO Bus: probed
[ 2.704830][ T1] libphy: Fixed MDIO Bus: probed
[ 2.715797][ T1] tun: Universal TUN/TAP device driver, 1.6
[ 2.715797][ T1] tun: Universal TUN/TAP device driver, 1.6
[ 2.727498][ T1] CAN device driver interface
[ 2.727498][ T1] CAN device driver interface
[ 2.738527][ T1] PPP generic driver version 2.4.2
[ 2.738527][ T1] PPP generic driver version 2.4.2
[ 2.748582][ T1] PPP BSD Compression module registered
[ 2.748582][ T1] PPP BSD Compression module registered
[ 2.759381][ T1] PPP Deflate Compression module registered
[ 2.759381][ T1] PPP Deflate Compression module registered
[ 2.770884][ T1] PPP MPPE Compression module registered
[ 2.770884][ T1] PPP MPPE Compression module registered
[ 2.781856][ T1] NET: Registered protocol family 24
[ 2.781856][ T1] NET: Registered protocol family 24
[ 2.792127][ T1] PPTP driver version 0.8.5
[ 2.792127][ T1] PPTP driver version 0.8.5
[ 2.801040][ T1] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.801040][ T1] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.815481][ T1] ehci-platform: EHCI generic platform driver
[ 2.815481][ T1] ehci-platform: EHCI generic platform driver
[ 2.827549][ T1] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 2.827549][ T1] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 2.841314][ T1] ohci-platform: OHCI generic platform driver
[ 2.841314][ T1] ohci-platform: OHCI generic platform driver
[ 2.853410][ T1] usbcore: registered new interface driver cdc_acm
[ 2.853410][ T1] usbcore: registered new interface driver cdc_acm
[ 2.866115][ T1] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 2.866115][ T1] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 2.883714][ T1] usbcore: registered new interface driver uas
[ 2.883714][ T1] usbcore: registered new interface driver uas
[ 2.895774][ T1] usbcore: registered new interface driver usb-storage
[ 2.895774][ T1] usbcore: registered new interface driver usb-storage
[ 2.909243][ T1] usbcore: registered new interface driver usbserial_generic
[ 2.909243][ T1] usbcore: registered new interface driver usbserial_generic
[ 2.923701][ T1] usbserial: USB Serial support registered for generic
[ 2.923701][ T1] usbserial: USB Serial support registered for generic
[ 2.937125][ T1] usbcore: registered new interface driver ftdi_sio
[ 2.937125][ T1] usbcore: registered new interface driver ftdi_sio
[ 2.950021][ T1] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 2.950021][ T1] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 2.966052][ T1] usbcore: registered new interface driver usb_serial_simple
[ 2.966052][ T1] usbcore: registered new interface driver usb_serial_simple
[ 2.980509][ T1] usbserial: USB Serial support registered for carelink
[ 2.980509][ T1] usbserial: USB Serial support registered for carelink
[ 2.994096][ T1] usbserial: USB Serial support registered for zio
[ 2.994096][ T1] usbserial: USB Serial support registered for zio
[ 3.006816][ T1] usbserial: USB Serial support registered for funsoft
[ 3.006816][ T1] usbserial: USB Serial support registered for funsoft
[ 3.020231][ T1] usbserial: USB Serial support registered for flashloader
[ 3.020231][ T1] usbserial: USB Serial support registered for flashloader
[ 3.034345][ T1] usbserial: USB Serial support registered for google
[ 3.034345][ T1] usbserial: USB Serial support registered for google
[ 3.047606][ T1] usbserial: USB Serial support registered for libtransistor
[ 3.047606][ T1] usbserial: USB Serial support registered for libtransistor
[ 3.062065][ T1] usbserial: USB Serial support registered for vivopay
[ 3.062065][ T1] usbserial: USB Serial support registered for vivopay
[ 3.075477][ T1] usbserial: USB Serial support registered for moto_modem
[ 3.075477][ T1] usbserial: USB Serial support registered for moto_modem
[ 3.089415][ T1] usbserial: USB Serial support registered for motorola_tetra
[ 3.089415][ T1] usbserial: USB Serial support registered for motorola_tetra
[ 3.104077][ T1] usbserial: USB Serial support registered for novatel_gps
[ 3.104077][ T1] usbserial: USB Serial support registered for novatel_gps
[ 3.118184][ T1] usbserial: USB Serial support registered for hp4x
[ 3.118184][ T1] usbserial: USB Serial support registered for hp4x
[ 3.131081][ T1] usbserial: USB Serial support registered for suunto
[ 3.131081][ T1] usbserial: USB Serial support registered for suunto
[ 3.144319][ T1] usbserial: USB Serial support registered for siemens_mpi
[ 3.144319][ T1] usbserial: USB Serial support registered for siemens_mpi
[ 3.158986][ T1] dummy_hcd dummy_hcd.0: USB Host+Gadget Emulator, driver 02 May 2005
[ 3.158986][ T1] dummy_hcd dummy_hcd.0: USB Host+Gadget Emulator, driver 02 May 2005
[ 3.175000][ T1] dummy_hcd dummy_hcd.0: Dummy host controller
[ 3.175000][ T1] dummy_hcd dummy_hcd.0: Dummy host controller
[ 3.187015][ T1] dummy_hcd dummy_hcd.0: new USB bus registered, assigned bus number 1
[ 3.187015][ T1] dummy_hcd dummy_hcd.0: new USB bus registered, assigned bus number 1
[ 3.203366][ T1] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[ 3.203366][ T1] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[ 3.221283][ T1] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 3.221283][ T1] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 3.237111][ T1] usb usb1: Product: Dummy host controller
[ 3.237111][ T1] usb usb1: Product: Dummy host controller
[ 3.248424][ T1] usb usb1: Manufacturer: Linux 5.10.72-00001-gcb6f328b5e81-dirty dummy_hcd
[ 3.248424][ T1] usb usb1: Manufacturer: Linux 5.10.72-00001-gcb6f328b5e81-dirty dummy_hcd
[ 3.265470][ T1] usb usb1: SerialNumber: dummy_hcd.0
[ 3.265470][ T1] usb usb1: SerialNumber: dummy_hcd.0
[ 3.276331][ T1] hub 1-0:1.0: USB hub found
[ 3.276331][ T1] hub 1-0:1.0: USB hub found
[ 3.285253][ T1] hub 1-0:1.0: 1 port detected
[ 3.285253][ T1] hub 1-0:1.0: 1 port detected
[ 3.295819][ T1] snvs_pwrkey 30370000.snvs:snvs-powerkey: snvs pwkey: failed to find trusty node. Use normal mode.
[ 3.295819][ T1] snvs_pwrkey 30370000.snvs:snvs-powerkey: snvs pwkey: failed to find trusty node. Use normal mode.
[ 3.317313][ T1] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/30000000.bus/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0
[ 3.317313][ T1] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/30000000.bus/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0
[ 3.344618][ T1] usbcore: registered new interface driver xpad
[ 3.344618][ T1] usbcore: registered new interface driver xpad
[ 3.356856][ T1] usbcore: registered new interface driver usb_acecad
[ 3.356856][ T1] usbcore: registered new interface driver usb_acecad
[ 3.370111][ T1] usbcore: registered new interface driver aiptek
[ 3.370111][ T1] usbcore: registered new interface driver aiptek
[ 3.382671][ T1] usbcore: registered new interface driver gtco
[ 3.382671][ T1] usbcore: registered new interface driver gtco
[ 3.394886][ T1] usbcore: registered new interface driver hanwang
[ 3.394886][ T1] usbcore: registered new interface driver hanwang
[ 3.407621][ T1] usbcore: registered new interface driver kbtab
[ 3.407621][ T1] usbcore: registered new interface driver kbtab
[ 3.420188][ T1] i2c /dev entries driver
[ 3.420188][ T1] i2c /dev entries driver
[ 3.429473][ T1] usbcore: registered new interface driver uvcvideo
[ 3.429473][ T1] usbcore: registered new interface driver uvcvideo
[ 3.442354][ T1] USB Video Class driver (1.1.1)
[ 3.442354][ T1] USB Video Class driver (1.1.1)
[ 3.451932][ T1] gspca_main: v2.14.0 registered
[ 3.451932][ T1] gspca_main: v2.14.0 registered
[ 3.461634][ T1] __power_supply_register: Expected proper parent device for 'battery'
[ 3.461634][ T1] __power_supply_register: Expected proper parent device for 'battery'
[ 3.478122][ T1] __power_supply_register: Expected proper parent device for 'usb'
[ 3.478122][ T1] __power_supply_register: Expected proper parent device for 'usb'
[ 3.496605][ T1] device-mapper: uevent: version 1.0.3
[ 3.496605][ T1] device-mapper: uevent: version 1.0.3
[ 3.507625][ T1] device-mapper: ioctl: 4.44.0-ioctl (2021-02-01) initialised: dm-devel@redhat.com
[ 3.507625][ T1] device-mapper: ioctl: 4.44.0-ioctl (2021-02-01) initialised: dm-devel@redhat.com
[ 3.527486][ T1] sdhci: Secure Digital Host Controller Interface driver
[ 3.527486][ T1] sdhci: Secure Digital Host Controller Interface driver
[ 3.541256][ T1] sdhci: Copyright(c) Pierre Ossman
[ 3.541256][ T1] sdhci: Copyright(c) Pierre Ossman
[ 3.551707][ T1] Synopsys Designware Multimedia Card Interface Driver
[ 3.551707][ T1] Synopsys Designware Multimedia Card Interface Driver
[ 3.565777][ T1] sdhci-pltfm: SDHCI platform and OF driver helper
[ 3.565777][ T1] sdhci-pltfm: SDHCI platform and OF driver helper
[ 3.581149][ T1] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 3.581149][ T1] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 3.595486][ T1] hid: raw HID events driver (C) Jiri Kosina
[ 3.595486][ T1] hid: raw HID events driver (C) Jiri Kosina
[ 3.609562][ T1] usbcore: registered new interface driver usbhid
[ 3.609562][ T1] usbcore: registered new interface driver usbhid
[ 3.610883][ T7] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA
[ 3.610883][ T7] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA
[ 3.611330][ T9] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA
[ 3.611330][ T9] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA
[ 3.622108][ T1] usbhid: USB HID core driver
[ 3.622108][ T1] usbhid: USB HID core driver
[ 3.623325][ T1] ashmem: initialized
[ 3.623325][ T1] ashmem: initialized
[ 3.673261][ T1] gnss: GNSS driver registered with major 504
[ 3.673261][ T1] gnss: GNSS driver registered with major 504
[ 3.688241][ T1] NET: Registered protocol family 26
[ 3.688241][ T1] NET: Registered protocol family 26
[ 3.698548][ T1] GACT probability NOT on
[ 3.698548][ T1] GACT probability NOT on
[ 3.706917][ T1] Mirror/redirect action on
[ 3.706917][ T1] Mirror/redirect action on
[ 3.715640][ T1] netem: version 1.3
[ 3.715640][ T1] netem: version 1.3
[ 3.723228][ T1] u32 classifier
[ 3.723228][ T1] u32 classifier
[ 3.730029][ T1] input device check on
[ 3.730029][ T1] input device check on
[ 3.738736][ T1] Actions configured
[ 3.738736][ T1] Actions configured
[ 3.740253][ T19] mmc2: new HS400 Enhanced strobe MMC card at address 0001
[ 3.740253][ T19] mmc2: new HS400 Enhanced strobe MMC card at address 0001
[ 3.747855][ T1] xt_time: kernel timezone is -0000
[ 3.747855][ T1] xt_time: kernel timezone is -0000
[ 3.762231][ T19] mmcblk2: mmc2:0001 DG4032 29.1 GiB
[ 3.762231][ T19] mmcblk2: mmc2:0001 DG4032 29.1 GiB
[ 3.771468][ T1] ipip: IPv4 and MPLS over IPv4 tunneling driver
[ 3.771468][ T1] ipip: IPv4 and MPLS over IPv4 tunneling driver
[ 3.781820][ T19] mmcblk2boot0: mmc2:0001 DG4032 partition 1 4.00 MiB
[ 3.781820][ T19] mmcblk2boot0: mmc2:0001 DG4032 partition 1 4.00 MiB
[ 3.794695][ T1] gre: GRE over IPv4 demultiplexor driver
[ 3.794695][ T1] gre: GRE over IPv4 demultiplexor driver
[ 3.807427][ T19] mmcblk2boot1: mmc2:0001 DG4032 partition 2 4.00 MiB
[ 3.807427][ T19] mmcblk2boot1: mmc2:0001 DG4032 partition 2 4.00 MiB
[ 3.818630][ T1] ip_gre: GRE over IPv4 tunneling driver
[ 3.818630][ T1] ip_gre: GRE over IPv4 tunneling driver
[ 3.831742][ T19] mmcblk2rpmb: mmc2:0001 DG4032 partition 3 16.0 MiB, chardev (508:0)
[ 3.831742][ T19] mmcblk2rpmb: mmc2:0001 DG4032 partition 3 16.0 MiB, chardev (508:0)
[ 3.843514][ T1] IPv4 over IPsec tunneling driver
[ 3.843514][ T1] IPv4 over IPsec tunneling driver
[ 3.861262][ T19] mmcblk2: p1 p2
[ 3.861262][ T19] mmcblk2: p1 p2
[ 3.869136][ T1] Initializing XFRM netlink socket
[ 3.869136][ T1] Initializing XFRM netlink socket
[ 3.885403][ T1] IPsec XFRM device driver
[ 3.885403][ T1] IPsec XFRM device driver
[ 3.894510][ T1] NET: Registered protocol family 10
[ 3.894510][ T1] NET: Registered protocol family 10
[ 3.906908][ T1] Segment Routing with IPv6
[ 3.906908][ T1] Segment Routing with IPv6
[ 3.915798][ T1] mip6: Mobile IPv6
[ 3.915798][ T1] mip6: Mobile IPv6
[ 3.923857][ T1] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 3.923857][ T1] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 3.937868][ T1] ip6_gre: GRE over IPv6 tunneling driver
[ 3.937868][ T1] ip6_gre: GRE over IPv6 tunneling driver
[ 3.949457][ T1] NET: Registered protocol family 17
[ 3.949457][ T1] NET: Registered protocol family 17
[ 3.959769][ T1] NET: Registered protocol family 15
[ 3.959769][ T1] NET: Registered protocol family 15
[ 3.970077][ T1] can: controller area network core
[ 3.970077][ T1] can: controller area network core
[ 3.980292][ T1] NET: Registered protocol family 29
[ 3.980292][ T1] NET: Registered protocol family 29
[ 3.990585][ T1] can: raw protocol
[ 3.990585][ T1] can: raw protocol
[ 3.997942][ T1] can: broadcast manager protocol
[ 3.997942][ T1] can: broadcast manager protocol
[ 4.007699][ T1] can: netlink gateway - max_hops=1
[ 4.007699][ T1] can: netlink gateway - max_hops=1
[ 4.017896][ T1] l2tp_core: L2TP core driver, V2.0
[ 4.017896][ T1] l2tp_core: L2TP core driver, V2.0
[ 4.028000][ T1] l2tp_ppp: PPPoL2TP kernel driver, V2.0
[ 4.028000][ T1] l2tp_ppp: PPPoL2TP kernel driver, V2.0
[ 4.038984][ T1] tipc: Activated (version 2.0.0)
[ 4.038984][ T1] tipc: Activated (version 2.0.0)
[ 4.048858][ T1] NET: Registered protocol family 30
[ 4.048858][ T1] NET: Registered protocol family 30
[ 4.059251][ T1] tipc: Started in single node mode
[ 4.059251][ T1] tipc: Started in single node mode
[ 4.075973][ T1] NET: Registered protocol family 36
[ 4.075973][ T1] NET: Registered protocol family 36
[ 4.086990][ T1] NET: Registered protocol family 40
[ 4.086990][ T1] NET: Registered protocol family 40
[ 4.098605][ T1] registered taskstats version 1
[ 4.098605][ T1] registered taskstats version 1
[ 4.108210][ T1] Loading compiled-in X.509 certificates
[ 4.108210][ T1] Loading compiled-in X.509 certificates
[ 4.119228][ T1] page_owner is disabled
[ 4.119228][ T1] page_owner is disabled
[ 4.127552][ T1] Key type ._fscrypt registered
[ 4.127552][ T1] Key type ._fscrypt registered
[ 4.136956][ T1] Key type .fscrypt registered
[ 4.136956][ T1] Key type .fscrypt registered
[ 4.146187][ T1] Key type fscrypt-provisioning registered
[ 4.146187][ T1] Key type fscrypt-provisioning registered
[ 4.158538][ T1] pstore: Using crash dump compression: deflate
[ 4.158538][ T1] pstore: Using crash dump compression: deflate
[ 4.224127][ T7] nxp-pca9450 0-0025: pca9450bc probed.
[ 4.224127][ T7] nxp-pca9450 0-0025: pca9450bc probed.
[ 4.235037][ T7] i2c i2c-0: IMX I2C adapter registered
[ 4.235037][ T7] i2c i2c-0: IMX I2C adapter registered
[ 4.248115][ T7] rtc-abx80x 1-0069: model 1805, revision 2.3, lot 10, wafer e, uid 4641
[ 4.248115][ T7] rtc-abx80x 1-0069: model 1805, revision 2.3, lot 10, wafer e, uid 4641
[ 4.267256][ T7] rtc-abx80x 1-0069: Oscillator failure, data is invalid.
[ 4.267256][ T7] rtc-abx80x 1-0069: Oscillator failure, data is invalid.
[ 4.281300][ T7] rtc-abx80x 1-0069: registered as rtc0
[ 4.281300][ T7] rtc-abx80x 1-0069: registered as rtc0
[ 4.292744][ T7] rtc-abx80x 1-0069: Oscillator failure, data is invalid.
[ 4.292744][ T7] rtc-abx80x 1-0069: Oscillator failure, data is invalid.
[ 4.306668][ T7] rtc-abx80x 1-0069: hctosys: unable to read the hardware clock
[ 4.306668][ T7] rtc-abx80x 1-0069: hctosys: unable to read the hardware clock
[ 4.321687][ T7] i2c i2c-1: IMX I2C adapter registered
[ 4.321687][ T7] i2c i2c-1: IMX I2C adapter registered
[ 4.333599][ T7] i2c i2c-4: IMX I2C adapter registered
[ 4.333599][ T7] i2c i2c-4: IMX I2C adapter registered
[ 4.345556][ T7] i2c i2c-5: IMX I2C adapter registered
[ 4.345556][ T7] i2c i2c-5: IMX I2C adapter registered
[ 4.357492][ T7] pwm-backlight dsi_backlight: supply power not found, using dummy regulator
[ 4.357492][ T7] pwm-backlight dsi_backlight: supply power not found, using dummy regulator
[ 4.378237][ T7] pwm-backlight lvds_backlight: supply power not found, using dummy regulator
[ 4.378237][ T7] pwm-backlight lvds_backlight: supply power not found, using dummy regulator
[ 4.402970][ T9] sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO
[ 4.402970][ T9] sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO
[ 4.406918][ T7] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 5 mkt segment 0 supported-hw 0x20 0x1
[ 4.406918][ T7] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 5 mkt segment 0 supported-hw 0x20 0x1
[ 4.442011][ T1] ALSA device list:
[ 4.442011][ T1] ALSA device list:
[ 4.449365][ T1] No soundcards found.
[ 4.449365][ T1] No soundcards found.
[ 4.450791][ T9] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
[ 4.450791][ T9] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
[ 4.474319][ T1] Freeing unused kernel memory: 3456K
[ 4.474319][ T1] Freeing unused kernel memory: 3456K
[ 4.484886][ T1] Run /init as init process
[ 4.484886][ T1] Run /init as init process
[ 4.485502][ C0] random: fast init done
[ 4.485502][ C0] random: fast init done
[ 4.528050][ T1] init: init first stage started!
[ 4.528050][ T1] init: init first stage started!
[ 4.537996][ T1] init: Unable to open /lib/modules, skipping module loading.
[ 4.537996][ T1] init: Unable to open /lib/modules, skipping module loading.
[ 4.538506][ T36] mmc1: host does not support reading read-only switch, assuming write-enable
[ 4.538506][ T36] mmc1: host does not support reading read-only switch, assuming write-enable
[ 4.553040][ T1] init: Switching root to '/first_stage_ramdisk'
[ 4.553040][ T1] init: Switching root to '/first_stage_ramdisk'
[ 4.582935][ T1] init: [libfs_mgr]ReadFstabFromDt(): failed to read fstab from dt
[ 4.582935][ T1] init: [libfs_mgr]ReadFstabFromDt(): failed to read fstab from dt
[ 4.599026][ T1] init: Using Android DT directory /proc/device-tree/firmware/android/
[ 4.599026][ T1] init: Using Android DT directory /proc/device-tree/firmware/android/
[ 4.700056][ T1] init: bool android::init::BlockDevInitializer::InitDevices(std::set<std::string>): partition(s) not found in /sys, waiting for their uevent(s): metadata
[ 4.700056][ T1] init: bool android::init::BlockDevInitializer::InitDevices(std::set<std::string>): partition(s) not found in /sys, waiting for their uevent(s): metadata
[ 4.707181][ T36] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
[ 4.707181][ T36] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
[ 4.746609][ T36] mmcblk1: mmc1:aaaa SE32G 29.7 GiB
[ 4.746609][ T36] mmcblk1: mmc1:aaaa SE32G 29.7 GiB
[ 4.762839][ T36] mmcblk1: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14
[ 4.762839][ T36] mmcblk1: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14
[ 14.743079][ T1] init: Wait for partitions returned after 10011ms
[ 14.743079][ T1] init: Wait for partitions returned after 10011ms
[ 14.756400][ T1] init: bool android::init::BlockDevInitializer::InitDevices(std::set<std::string>): partition(s) not found after polling timeout: metadata
[ 14.756400][ T1] init: bool android::init::BlockDevInitializer::InitDevices(std::set<std::string>): partition(s) not found after polling timeout: metadata
[ 14.786735][ T1] init: Failed to mount required partitions early ...
[ 14.786735][ T1] init: Failed to mount required partitions early ...
[ 14.808516][ T1] init: InitFatalReboot: signal 6
[ 14.808516][ T1] init: InitFatalReboot: signal 6
[ 14.833756][ T1] init: #00 pc 00000000000b0008 /system/bin/init
[ 14.833756][ T1] init: #00 pc 00000000000b0008 /system/bin/init
[ 14.846748][ T1] init: #01 pc 000000000004cd90 /system/bin/init
[ 14.846748][ T1] init: #01 pc 000000000004cd90 /system/bin/init
[ 14.859330][ T1] init: #02 pc 0000000000013ab0 /system/lib64/libbase.so
[ 14.859330][ T1] init: #02 pc 0000000000013ab0 /system/lib64/libbase.so
[ 14.873279][ T1] init: #03 pc 0000000000013090 /system/lib64/libbase.so
[ 14.873279][ T1] init: #03 pc 0000000000013090 /system/lib64/libbase.so
[ 14.887239][ T1] init: #04 pc 0000000000075b1c /system/bin/init
[ 14.887239][ T1] init: #04 pc 0000000000075b1c /system/bin/init
[ 14.899793][ T1] init: #05 pc 000000000002e0ec /system/bin/init
[ 14.899793][ T1] init: #05 pc 000000000002e0ec /system/bin/init
[ 14.912593][ T1] kvm: exiting hardware virtualization
[ 14.912593][ T1] kvm: exiting hardware virtualization
[ 14.967756][ T1] imx2-wdt 30280000.watchdog: Device shutdown: Expect reboot!
[ 14.967756][ T1] imx2-wdt 30280000.watchdog: Device shutdown: Expect reboot!
[ 14.983297][ T1] reboot: Restarting system with command 'bootloader'
[ 14.983297][ T1] reboot: Restarting system with command 'bootloader'

U-Boot SPL 2021.04-00001-g302084ead7-dirty (Mar 27 2022 - 14:18:05 +0530)
DDRINFO: Cfg attempt: [ 3/4 ]
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
==============================================================================

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

3,168件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Did you try emmc boot?

0 件の賞賛
返信

3,166件の閲覧回数
swapnilpendhare
Contributor III

We are not touching EMMC for now and just trying it from SD Card, 

0 件の賞賛
返信