Just add SD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Just add SD

Jump to solution
2,133 Views
farworld
Contributor I

Hello once again forum,

Just wanting to ask, is it possible I could just set the Sabre-lite, or a marsboard up to just boot from the micro SD?

If so, some actual instructions beyond 'Oh, look at the manual written for actual experts' would be nice.

Labels (3)
0 Kudos
Reply
1 Solution
2,028 Views
EricNelson
Senior Contributor II
0 Kudos
Reply
5 Replies
2,028 Views
farworld
Contributor I

So, you're saying that all I needed to do, was load the images onto the SD card and it would simply boot from them?

0 Kudos
Reply
2,029 Views
EricNelson
Senior Contributor II

Yes.

0 Kudos
Reply
2,028 Views
farworld
Contributor I

Thank you. You've pretty much just made my day with that.

0 Kudos
Reply
2,028 Views
EricNelson
Senior Contributor II

Glad to hear it.

Enjoy!

0 Kudos
Reply
2,028 Views
EricNelson
Senior Contributor II

Hi Luke,

What do you mean by "just boot from the microSD"?

The SABRE Lite essentially does that. What I mean is that all boot instructions are on the card in the boot script (6x_bootscript).

We have boot scripts that load Windows Embedded, Android, QNX, Yocto, Timesys, Ubuntu, Debian, et cetera and switch between them simply swapping cards.

You can also force the boot loader to load from SD, but this is a tricky operation, and recommended only for 'actual experts'...

0 Kudos
Reply