Just add SD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Just add SD

跳至解决方案
2,391 次查看
farworld
Contributor I

Hello once again forum,

Just wanting to ask, is it possible I could just set the Sabre-lite, or a marsboard up to just boot from the micro SD?

If so, some actual instructions beyond 'Oh, look at the manual written for actual experts' would be nice.

标签 (3)
0 项奖励
回复
1 解答
2,286 次查看
EricNelson
Senior Contributor II
0 项奖励
回复
5 回复数
2,286 次查看
farworld
Contributor I

So, you're saying that all I needed to do, was load the images onto the SD card and it would simply boot from them?

0 项奖励
回复
2,287 次查看
EricNelson
Senior Contributor II

Yes.

0 项奖励
回复
2,286 次查看
farworld
Contributor I

Thank you. You've pretty much just made my day with that.

0 项奖励
回复
2,286 次查看
EricNelson
Senior Contributor II

Glad to hear it.

Enjoy!

0 项奖励
回复
2,286 次查看
EricNelson
Senior Contributor II

Hi Luke,

What do you mean by "just boot from the microSD"?

The SABRE Lite essentially does that. What I mean is that all boot instructions are on the card in the boot script (6x_bootscript).

We have boot scripts that load Windows Embedded, Android, QNX, Yocto, Timesys, Ubuntu, Debian, et cetera and switch between them simply swapping cards.

You can also force the boot loader to load from SD, but this is a tricky operation, and recommended only for 'actual experts'...

0 项奖励
回复