Jiter 0.4.1 pypi package failed to build in yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Jiter 0.4.1 pypi package failed to build in yocto

1,677 次查看
taabouri
Contributor I

 

this is my first time with a rust package it’s jiter 0.4.1 that got from pypi.org i am trying to integrate this recipe with my tdx-reference-multimedia-image but it insist on failing this is the structure of the project:
── Cargo.lock
├── Cargo.toml
├── crates
│ ├── jiter
│ │ ├── benches
│ │ │ ├── bigints_array.json
│ │ │ ├── floats_array.json
│ │ │ ├── generate_big.py
│ │ │ ├── main.rs
│ │ │ ├── massive_ints_array.json
│ │ │ ├── medium_response.json
│ │ │ ├── pass1.json
│ │ │ ├── pass2.json
│ │ │ ├── python.rs
│ │ │ ├── sentence.json
│ │ │ ├── short_numbers.json
│ │ │ ├── string_array.json
│ │ │ ├── string_array_unique.json
│ │ │ ├── true_array.json
│ │ │ ├── true_object.json
│ │ │ ├── unicode.json
│ │ │ └── x100.json
│ │ ├── build.rs
│ │ ├── Cargo.toml
│ │ ├── LICENSE
│ │ ├── README.md
│ │ ├── src
│ │ │ ├── errors.rs
│ │ │ ├── jiter.rs
│ │ │ ├── lazy_index_map.rs
│ │ │ ├── lib.rs
│ │ │ ├── number_decoder.rs
│ │ │ ├── parse.rs
│ │ │ ├── py_lossless_float.rs
│ │ │ ├── py_string_cache.rs
│ │ │ ├── python.rs
│ │ │ ├── simd_aarch64.rs
│ │ │ ├── string_decoder.rs
│ │ │ └── value.rs
│ │ └── tests
│ │ ├── main.rs
│ │ └── python.rs
│ └── jiter-python
│ ├── bench.py
│ ├── Cargo.toml
│ ├── jiter.pyi
│ ├── README.md
│ ├── requirements.txt
│ ├── src
│ │ └── lib.rs
│ └── tests
│ ├── requirements.txt
│ └── test_jiter.py
├── oe-logs → /home/rania/pixii_os/pixii_os/build/tmp/work/cortexa72-cortexa53-tdx-linux/python3-jiter/0.4.1-r0/temp
├── oe-workdir → /home/rania/pixii_os/pixii_os/build/tmp/work/cortexa72-cortexa53-tdx-linux/python3-jiter/0.4.1-r0
├── PKG-INFO
├── pyproject.toml
└── README.md

this is the cargo.toml within crates/jiter:

[package]
name = "jiter"
description = "Fast Iterable JSON parser"
readme = "../../README.md"
authors = ["Samuel Colvin <samuel@pydantic.dev>"]
version = "0.4.1"
edition = "2021"
license = "MIT"
keywords = ["JSON", "parsing", "deserialization", "iter"]
categories = ["parser-implementations", "parsing"]
homepage = "https://github.com/pydantic/jiter/"
repository = "https://github.com/pydantic/jiter/"

[dependencies]
num-bigint = "0.4.4"
num-traits = "0.2.16"
ahash = "0.8.0"
smallvec = "1.11.0"
pyo3 = { version = "0.21.0", optional = true }
lexical-parse-float = { version = "0.8.5", features =  ["format"] }
bitvec = "1.0.1"

[features]
python = ["pyo3", "pyo3-build-config"]

[dev-dependencies]
bencher = "0.1.5"
paste = "1.0.7"
serde_json = {version = "1.0.87", features = ["preserve_order", "arbitrary_precision", "float_roundtrip"]}
serde = "1.0.147"
pyo3 = { workspace = true, default-features=false, features = ["num-bigint", "auto-initialize"] }
codspeed-bencher-compat = "2.3.1"

[build-dependencies]
pyo3-build-config = { version = "0.21.0", optional = true }

[[test]]
name = "python"
required-features = ["python"]

[[bench]]
name = "main"
harness = false

[[bench]]
name = "python"
required-features = ["python"]
harness = false

# get docs.rs to include python docs
[package.metadata.docs.rs]
all-features = true

[lints.clippy]
dbg_macro = "deny"
print_stdout = "deny"
print_stderr = "deny"
# in general we lint against the pedantic group, but we will whitelist
# certain lints which we don't want to enforce (for now)
pedantic = { level = "deny", priority = -1 }
missing_errors_doc = "allow"
module_name_repetitions = "allow"
must_use_candidate = "allow"
if_not_else = "allow"
cast_lossless = "allow"
cast_possible_wrap = "allow"
cast_possible_truncation = "allow"
cast_precision_loss = "allow"
match_bool = "allow"
doc_markdown = "allow"
implicit_clone = "allow"
iter_without_into_iter = "allow"
return_self_not_must_use = "allow"
inline_always = "allow"  # TODO remove?
match_same_arms = "allow"  # TODO remove?

and these are logs :

 

 

 

 
DEBUG: Executing shell function do_compile NOTE: cargo = /home/rania/pixii_os/pixii_os/build/tmp/work/cortexa72-cortexa53-tdx-linux/python3-jiter/0.4.1-r0/recipe-sysroot-native/usr/bin/cargo NOTE: rustc = NOTE: cargo build -v --target aarch64-tdx-linux --release --manifest-path=/home/rania/pixii_os/pixii_os/build/workspace/sources/python3-jiter//Cargo.toml warning: /home/rania/pixii_os/pixii_os/build/workspace/sources/python3-jiter/crates/jiter/Cargo.toml: dependency (pyo3) specified without providing a local path, Git repository, or version to use. This will be considered an error in future versions warning: /home/rania/pixii_os/pixii_os/build/workspace/sources/python3-jiter/crates/jiter/Cargo.toml: unused manifest key: dev-dependencies.pyo3.workspace warning: /home/rania/pixii_os/pixii_os/build/workspace/sources/python3-jiter/crates/jiter/Cargo.toml: unused manifest key: lints warning: /home/rania/pixii_os/pixii_os/build/workspace/sources/python3-jiter/Cargo.toml: unused manifest key: workspace.dependencies warning: /home/rania/pixii_os/pixii_os/build/workspace/sources/python3-jiter/Cargo.toml: unused manifest key: workspace.package warning: /home/rania/pixii_os/pixii_os/build/workspace/sources/python3-jiter/crates/jiter-python/Cargo.toml: d**ependency (pyo3) specified without providing a local path, Git repository, or version to use**. This will be considered an error in future versions warning: /home/rania/pixii_os/pixii_os/build/workspace/sources/python3-jiter/crates/jiter-python/Cargo.toml: unused manifest key: dependencies.pyo3.workspace warning: /home/rania/pixii_os/pixii_os/build/workspace/sources/python3-jiter/crates/jiter-python/Cargo.toml: unused manifest key: lints error: **no matching package named pyo3 found location searched: registry crates-io required by package jiter-python v0.4.1 (/home/rania/pixii_os/pixii_os/build/workspace/sources/python3-jiter/crates/jiter-python)** WARNING: exit code 101 from a shell command

this is the main cargo.toml within python3-jiter :

 

 

 

 
[workspace]
members = ["crates/jiter-python"]
resolver = "2"

[workspace.package]
authors = ["Samuel Colvin <samuel@pydantic.dev>"]
version = "0.4.1"
edition = "2021"
license = "MIT"
keywords = ["JSON", "parsing", "deserialization", "iter"]
categories = ["parser-implementations", "parsing"]
homepage = "https://github.com/pydantic/jiter/"
repository = "https://github.com/pydantic/jiter/"

[profile.bench]
debug = true
lto = true
opt-level = 3
codegen-units = 1

[profile.profiling]
inherits = "release"
debug = true

[workspace.dependencies]
pyo3 = { version = "0.21.0", default-features = false}

also this is the recipe :

LICENSE = “MIT” 
LIC_FILES_CHKSUM = “file://crates/jiter/LICENSE;md5=aa97bb3778992892e226b4504b83b60c” SRC_URI = “https://files.pythonhosted.org/packages/f6/27/53d3ffa863e7ef40023b1730fc5c999a616f3695145fd6fd7a351e8a8ae7/jiter-${PV}.tar.gz 1” 
SRC_URI[md5sum] = “98a4910b537b4c71b0eb29afe4c4b45e” SRC_URI[sha1sum] = “8f77c34d415ce96cf9cf275359f3e569a16e8786” 
SRC_URI[sha256sum] = “741851cf5f37cf3583f2a56829d734c9fd17334770c9a326e6d25291603d4278” SRC_URI[sha384sum] = “2495d36b80d62232213f1b4ec57f6ffb7008172f308bdb739321a72d5c2290b89aab469c2178c0be2e8b2e4f3a48ca07” 
SRC_URI[sha512sum] = “420f7e6785bb34441f27476bad7abc5a362ca98735d527bd90b5980951a0b3116926d82863bab4d12769e42d0e70b783e494bb90e30ae4edc035752289875e42” 
S = “${WORKDIR}/jiter-${PV}” 
inherit cargo pypi
 PYPI_PACKAGE = “jiter”  

 

0 项奖励
回复
3 回复数

1,648 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Which board are you using? which yocto? i will try to reproduce it.

Regards

0 项奖励
回复

1,645 次查看
taabouri
Contributor I

imy board is apalis imx8 quad max

i am using yocto kirkstone

could u please try it from your side and tell me what u did exactly cause i literally tried everything 

0 项奖励
回复

1,618 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

I do not have Apalis board you should check with them this issue.

Regards

0 项奖励
回复