Java SE on imx25

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Java SE on imx25

4,169件の閲覧回数
erhan14
Contributor I

Hi,

I want to add Java SE support using OpenJDK with Cacao VM to imx258 demo board.

How can I configure ltib to prepare a flash image with Java support?

Thanks

ラベル(2)
タグ(3)
0 件の賞賛
返信
7 返答(返信)

3,857件の閲覧回数
OtavioSalvador
Senior Contributor II

If you are open to work in adding i.MX25 support in Yocto Project BSP (see FSL Community BSP) the later Java addition is quite trivial. We have the meta-java that has all this done and provides several Open Source VM alternatives.

Currently the i.MX25 is not supported by the BSP, that's why I put this remark there.

0 件の賞賛
返信

3,857件の閲覧回数
erhan14
Contributor I

Is there a step by step guide for porting the official BSP to Yocto based one?

0 件の賞賛
返信

3,857件の閲覧回数
OtavioSalvador
Senior Contributor II

No; there's no such guide yet.

I can try to help if you want. Otherwise you can hire us (or someone else) to do the work. Either way works.

Initial support using mainline kernel and mainline U-Boot should be trivial. The i.MX25 2.6.31 kernel might be a little bit more problematic (due the fixes need for toolchain compatibility and others) but also doable.

0 件の賞賛
返信

3,857件の閲覧回数
erhan14
Contributor I

Freescale released official Yocto release but I cannot find imx25 port in it?

0 件の賞賛
返信

3,857件の閲覧回数
OtavioSalvador
Senior Contributor II

As I said previously it has not been added.

Someone needs (or sponsor a company) to do it and maintain it.

0 件の賞賛
返信

3,857件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please use the following from Community :

“All Boards Java”

https://community.freescale.com/docs/DOC-1478

Note, for i.MX25 we should use ARMv5 packages :

http://www.oracle.com/technetwork/java/embedded/downloads/javase/index.html

0 件の賞賛
返信

3,857件の閲覧回数
erhan14
Contributor I

Hi,

Thanks for the quick response.

I actually want to use opensource VM alternatives as Oracle Java is licensed for embedded use.

Thanks

0 件の賞賛
返信