Jailhouse porting onto imx.8mq

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Jailhouse porting onto imx.8mq

570 Views
MEGHANAB
Contributor I

For the i.MX 8MQ prebuilt image provided,does it include jailhouse hypervisor,the required kernel modules(jailhouse.ko,uio_ivshmem.ko),and guest os cell configuration.If yes pls provide the link for the prebuilt image
Regards
Meghana

0 Kudos
Reply
4 Replies

552 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @MEGHANAB 

 

I hope you are doing very well.

 

Please refer to the chapter 5.6.11 Building Jailhouse of the i.MX Yocto Project User's Guide.

There is described how to build Jailhouse for i.MX8MQ.

 

Best regards,

Salas.

0 Kudos
Reply

533 Views
MEGHANAB
Contributor I
Please mention which linux bsp is supported for imx8mq jailhouse.
Regards
0 Kudos
Reply

508 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @MEGHANAB 

 

The version that you are using is compatible with Jailhouse Hypervisor.

How did you flashed your image?

 

Best regards,

Salas.

0 Kudos
Reply

536 Views
MEGHANAB
Contributor I

So, Should i have to build the image with yocto instead of using prebuilt one?
But when I'm booting the prebuilt image the board is not getting booted.I have used LF_v6.12.3-1.0.0_images_IMX8MQEVK.Please do the needful.
Thank you

0 Kudos
Reply