J1939 support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

J1939 support

1,804件の閲覧回数
kishorekrish
Contributor I

Hi,

Is J1939 protocol supports on your IMX6Q6AVT please explain me..

Thank you.

ラベル(4)
0 件の賞賛
返信
1 返信

1,531件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi kishore krish,

Yes,J1939 is a higher-layer protocol based on Controller Area Network (CAN). J1939 apparently uses the CAN 2.0b specification which is the same as what is supported in the FlexCAN module of the MX6Q (the 29-bit extended operation of CAN 2.0b).
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信