J1939 support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

J1939 support

1,749 Views
kishorekrish
Contributor I

Hi,

Is J1939 protocol supports on your IMX6Q6AVT please explain me..

Thank you.

0 Kudos
Reply
1 Reply

1,476 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi kishore krish,

Yes,J1939 is a higher-layer protocol based on Controller Area Network (CAN). J1939 apparently uses the CAN 2.0b specification which is the same as what is supported in the FlexCAN module of the MX6Q (the 29-bit extended operation of CAN 2.0b).
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply