Issues with serial on iMX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issues with serial on iMX6

832 次查看
bogdananton
Contributor I

Hello we use iMX6DP4AVT1AA  devices in a hardware setup running on windows7 32bit and libusbx-1.0.15-win 

We face some problems on the serial hardware, where we have a FTDI232RL + 3.3V level translation  to comunicate with the iMX chip  .

Sometimes the test system fails when waiting  for  iMX boot console response. 

Is there any hardware alternative to ftdi232rl chip for comunication with imx?

We tryied a alternative using the native COM1  via a max232 + optical isolation and level translation, but the results where worst 

Any sugestions?

Thank you

0 项奖励
回复
1 回复

785 次查看
igorpadykov
NXP Employee
NXP Employee

Hi bogdan

from i.MX6 side there are no restrictions, one can use any rs232

converter or USB to serial UART interface.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复