Issues with Android Boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issues with Android Boot

1,144件の閲覧回数
anurag16doshi
Contributor III

I am using imx8mn board. I had a working Android boot img running. I made changes and redid the booting. I am working on Ubuntu 16.04 which is part of a dual booted PC. The allocated memory for the linux machine is 200+ GB. After remaking the kernel and boot images. My Ubuntu has run out of space. The main bulk of the memory is being used by .intermediate folder in <directory>/out/soong/.intermediate

 

I have used a procedure as mentioned in my previous post. https://community.nxp.com/t5/i-MX-Processors/Building-Android-BSP-with-RPMsg-enabled-for-iMX8-Nano/m...

 

I am uncertain of what the issue is. Could someone help understand the same?

 

TIA,

Anurag

0 件の賞賛
返信
1 返信

1,131件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Anurag16doshi,

The android BSP is not tested on ubuntu 16 you can try ubuntu 18, and it takes aprox 150GB, do not know exactly why it takes too much in your computer but you must deleted everything before compiled again.

 

Regards

 

 

0 件の賞賛
返信