Issues in camera after enabling MIPI-DSI in IMX8MP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues in camera after enabling MIPI-DSI in IMX8MP

Jump to solution
5,413 Views
ashlinsurey_a
Contributor II

Hi,

 

We have designed a carrier board (based on Variscite IMX8MP DART SOM) with 1 MIPI CSI camera and 1 MIPI DSI display.
When adding support for both camera and DSI display, the display works fine but we are unable to capture frames from the camera (camera driver loads correctly).
If we remove/disable the MIPI DSI display entry from the DTB, we can capture images from the camera. 

MIPI DSI Display entry:

/* MIPI-DSI */

&lcdif1 {
        status = "okay";
}; 

&mipi_dsi {
        status = "okay";
        /* DISPLAY */
        panel@0 {
                compatible = "techstar,ts8550b";
                reg = <0>;
                pinctrl-0 = <&pinctrl_mipi_dsi_en>;
                reset-gpio = <&gpio1 12 GPIO_ACTIVE_HIGH>;
                dsi-lanes = <2>;
                video-mode = <2>;
                panel-width-mm = <68>; //TBC
                panel-height-mm = <121>; //TBC
                status = "okay";
        };
};


Camera driver entry:

&i2c2 { 
        clock-frequency = <400000>;
        pinctrl-names = "default", "gpio";
        pinctrl-0 = <&pinctrl_i2c2>;
        pinctrl-1 = <&pinctrl_i2c2_gpio>;
        scl-gpios = <&gpio5 16 GPIO_ACTIVE_HIGH>;
        sda-gpios = <&gpio5 17 GPIO_ACTIVE_HIGH>;
        status = "okay";

         ov2311_mipi1: ov2311_mipi1@42 {
                compatible = "ov2311";
                reg = <0x42>;
                clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;

                clock-names = "xclk";
/* Disabled CLKO2, since DART-MX8MP camera expansion board uses
* its own oscillator. Enable CLK02 if your desing requres it
*/
#if 0
                assigned-clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
                assigned-clock-parents = <&clk IMX8MP_CLK_24M>;
#endif
                assigned-clock-rates = <24000000>;
                mipi-data-lanes = <2>;
                camera-mipi-clk = <832>;
                csi_id = <0>;
                pinctrl-names = "default";
                pwn-gpios = <&gpio3 8 GPIO_ACTIVE_HIGH>;
                rst-gpios = <&gpio3 7 GPIO_ACTIVE_LOW>;
                mclk = <24000000>;
                mclk_source = <0>;
                mipi_csi;
                status = "okay";

                 port {
                        ov2311_mipi1_ep: endpoint {
                                remote-endpoint = <&mipi_csi0_ep>;
                                data-lanes = <1 2>;
                                clock-lanes = <0>;
                        };
                };
        };
};

 &mipi_csi_0 {
        #address-cells = <1>;
        #size-cells = <0>;
        status = "okay";

         port@0 {
                reg = <0>;
                mipi_csi0_ep: endpoint {
                        remote-endpoint = <&ov2311_mipi1_ep>;
                        data-lanes = <2>;
                        csis-hs-settle = <13>;
                        csis-clk-settle = <2>;
                        csis-wclk;
                };
        };
};

Are we missing something to use both MIPI CSI and MIPI DSI simultaneously? 

Attached dmesg log.

Thanks.

0 Kudos
Reply
1 Solution
5,323 Views
ashlinsurey_a
Contributor II

Hi,

We are using a monochrome camera with Y data only. So, we have used ISI. Also, we have a positive improvement.

We changed the sensor mipi clock from continuous to gated clock mode. We can stream the camera and mipi dsi simultaneously now. We are still facing issues in streaming the maximum sensor resolution[1600x1300], but this resolution is not essential for our use case. Thanks for your support.

View solution in original post

0 Kudos
Reply
7 Replies
5,399 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the logfile, did you use dual camera? could you bring up one camera to the mipi dsi? and what interface do you use? isi or isp? pls share the whole logfile, but you used the third party company source code, I'm not sure what difference between this from nxp bsp, but I can check it

0 Kudos
Reply
5,378 Views
ashlinsurey_a
Contributor II

Hi,

We are using only one camera. We removed the other camera entry in the dtb and checked. We are still facing the issue with one camera and mipi dsi setup. We are using isi. Can you specify the logs that you need?

0 Kudos
Reply
5,370 Views
joanxie
NXP TechSupport
NXP TechSupport

what is your camera format? raw12 bits? pls share your boot up logfile and your whole dts file

0 Kudos
Reply
5,357 Views
ashlinsurey_a
Contributor II

Hi,

We are using GREY format configured as RAW8. Attached the log and dts files.

From the log we get "CSIS_DPHYSTATUS[20]: 0x000000c1". From the TRM it means the clock lane is in stop state. In the working scenario, the value is "CSIS_DPHYSTATUS[20]: 0x000000c0". Is there a way to change the clock state?

0 Kudos
Reply
5,341 Views
joanxie
NXP TechSupport
NXP TechSupport

since you use raw data, why don't use ISP? if you use ISI, you need change the driver and imx8mp couldn't handle raw data directly, otherwise you have operation to handle this

0 Kudos
Reply
5,324 Views
ashlinsurey_a
Contributor II

Hi,

We are using a monochrome camera with Y data only. So, we have used ISI. Also, we have a positive improvement.

We changed the sensor mipi clock from continuous to gated clock mode. We can stream the camera and mipi dsi simultaneously now. We are still facing issues in streaming the maximum sensor resolution[1600x1300], but this resolution is not essential for our use case. Thanks for your support.

0 Kudos
Reply
4,117 Views
rumozhizheng
Contributor I

Hi,

    We are using a monochrome camera with Y too,I wonder how you solved the problem in the end。

0 Kudos
Reply