Issues about Uboot CMD on uboot 2014.04

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues about Uboot CMD on uboot 2014.04

1,551 Views
tony_l_cai
Contributor III

Hi all,

       I dont know what some Uboot cmd can be applied to on MX6DL Uboot 2014.04,such as

          loop    - infinite loop on address range

       This cmd will read the memory addr range as fast as possible,it's a infinite loop, but I dont know if it is meaningful,some articles say it can used for ddr test, I cannot understand it.

       help me,Thank you ~

Labels (3)
0 Kudos
Reply
5 Replies

1,407 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Tony,

About the ddr test you can refer to i.MX6/7 DDR Stress Test Tool V2.40 .

Have a great day,

Dan

0 Kudos
Reply

1,407 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi tony,

Which version BSP are you using?
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,407 Views
tony_l_cai
Contributor III

uboot 2014.04

kernel  Linux version 3.10.53

Android l5.0.0_1.0.0-ga

sorry I dont know whats your meaning about bsp version, hope the above can help you.

Now my problem is unsolved.

Thank you~

0 Kudos
Reply

1,407 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi tony,

The Android l5.0.0_1.0.0-ga is your BSP version. I will confirm your question for you. Here can you tell me the board you are using is the board you buy from our company or you designed it yourself?

Best Regards

Dan

0 Kudos
Reply

1,407 Views
tony_l_cai
Contributor III

Hi, wang

    Designed by ourselves.

0 Kudos
Reply