Issues about RTC on MX6DL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issues about RTC on MX6DL

1,280件の閲覧回数
tony_l_cai
Contributor III

Hi,All

     Now we should implement the function that Powering up by the timer when the system is on Power OFF state.Could the MX6DL can support the function? If support,how to implement?

3Q~

ラベル(3)
0 件の賞賛
返信
1 返信

1,228件の閲覧回数
Yuri
NXP Employee
NXP Employee

  You may look at  Chapter 22 [Low-level Power Management (PM) Driver],

section 22.1.1 (Software Operation) of “i.MX_6_Linux_Reference_Manual.pdf”

in Linux documentation how to treat with DORMANT (Power off) mode.

http://www.freescale.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&Parent_nodeId=13376994810...

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信