Issues about RTC on MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues about RTC on MX6DL

1,248 Views
tony_l_cai
Contributor III

Hi,All

     Now we should implement the function that Powering up by the timer when the system is on Power OFF state.Could the MX6DL can support the function? If support,how to implement?

3Q~

Labels (3)
0 Kudos
Reply
1 Reply

1,196 Views
Yuri
NXP Employee
NXP Employee

  You may look at  Chapter 22 [Low-level Power Management (PM) Driver],

section 22.1.1 (Software Operation) of “i.MX_6_Linux_Reference_Manual.pdf”

in Linux documentation how to treat with DORMANT (Power off) mode.

http://www.freescale.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&Parent_nodeId=13376994810...

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply