Hi, all
The first time I downloaded success, and then I want to start up the board. But it could not work. So I downloaded again,but it stop on the "Load u-boot" ,when I tried again, the same result appeared. Then I checked the DDR, The result is following:
MX6SL opened.
Write to HidMX6x failed.
rom_check_hab: writing cmd to device failed and error code is 997
rom_check_hab() failed.Please make sure board connected and in serial download mode.
What's wrong?
3Q~
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi tony
such time to time instability may be caused by
hardware: one can check Chapter 8 Avoiding Board Bring-up Problems
IMX6DQ6SDLHDG and test basic board functionality with SDK
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------