Issues about MFG Tool Log

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issues about MFG Tool Log

846 次查看
tony_l_cai
Contributor III

Dear All,

     Now I am porting the Android 5.0 on MX6DL,and refer to the i.MX 6Dual/6Quad BSP Porting Guide.pdf, I have ported the uboot. but after MFG downloading ,the uboot excuted failed, from the below MFG log, what's wrong with the steps in uboot porting maybe??  3Q~

pastedImage_1.png

DLL version: 2.2.3

Monday, July 13, 2015 09:19:24   Start new logging

ModuleID[2] LevelID[10]: CMyExceptionHandler thread is running

ModuleID[2] LevelID[1]: new MxHidDeviceClass

ModuleID[2] LevelID[10]: new MxHidDevice[02786C28]

ModuleID[2] LevelID[10]: Device Manager thread is running

ModuleID[2] LevelID[10]: CmdOperation[0] device chagned and reset to state 0

ModuleID[2] LevelID[10]: ExecuteCommand--Boot[WndIndex:0], File is D:\workbench\EM70_100\MFG\Mfgtools_20150121\Profiles\MX6DL Linux Update\OS Firmware\u-boot.bin

ModuleID[2] LevelID[1]: PortMgrDlg(0)--MxHidDevice--Command Boot excute failed

ModuleID[2] LevelID[10]: CmdOperation[0], current command executed failed, so SetEvent(hDevCanDeleteEvent)

标签 (3)
0 项奖励
回复
0 回复数