Issues about DDR Freq on Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues about DDR Freq on Boot

1,481 Views
tony_l_cai
Contributor III

Hi all,

     How can I get the DDR Freq on u-boot stage? And I want to know the DDR freq on u-boot. I also want to change the DDR Freq to the max freq, can you help me?3Q~

Labels (3)
0 Kudos
Reply
1 Reply

1,341 Views
Yuri
NXP Employee
NXP Employee

  You may use U-boot command “clocks” to get information about DDR frequency.

To change default after reset configuration of i.MX6, DCD table may be used.

Please look at the following :

“Need to modify the "flash_headers.h" file from u-boot for DDR3 modification”

https://community.freescale.com/message/548227#548227

Also, please refer to i.MX6 Reference Manual, boot chapter for more details.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply