I am working with linux kernel 2.6.31. The hardware is designed as per the imx28 schematics but the sdcard is a micro sdcard host instead of sdcard host in mx28.
These are the changes made to the BSP
our sdcard host is having four data lines only so i have removed SSP0_DATA4 - SSP0_DATA7 from the BSP of our custom board. I have also checked the SSP0_DETECT pin also it is connected properly only.
What i have understood after reading that when we connect a SD card , the SSP0_DETECT pin should go low. But this is not happening with our board.