Issues About DDR Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issues About DDR Configuration

1,653件の閲覧回数
tony_l_cai
Contributor III

Hi All,

     After filling the blanks About the Aid,I found not all params in the Aid are filled into the flash_header.s. And not all params in the flash_header.s can be found in the Aid script.So I want to know how to handle the relation between flash_header.s and Aid script.

     Another question, I use the ddr stress tool to  DDR frequency calibration, but after the number of loop cycle is up to 1479, the ddr haven't finish its test. And I want to know how many times this loop test need ?

     3q!

ラベル(2)
タグ(5)
0 件の賞賛
返信
1 返信

1,481件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tony

please look at document below describing ddr test usage

i.Mx6DQSDL DDR3 Script Aid

after passing calibration ddr test runs in endless loop.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信