Issue with the Kirkstone OS build when adding Qt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with the Kirkstone OS build when adding Qt

239 Views
tusharvernekar
Contributor II

Hello All,

I am building kirkstone OS 5.15 , whenever i add any QT packages(qtbase) in local.conf and do core-image-minimal . i get the following errors

| FAILED: src/tools/bootstrap/CMakeFiles/Bootstrap.dir/__/__/corelib/text/qlocale_tools.cpp.o

imx-yocto/build-xwayland-imx8mpsolidrun/tmp/work/x86_64-linux/qtbase-native/6.3.2-r0/git/src/corelib/text/qlocale_tools.cpp:57:10: fatal error: charconv: No such file or directory
| #include <charconv>

imx-yocto/build-xwayland-imx8mpsolidrun/tmp/work/x86_64-linux/qtbase-native/6.3.2-r0/git/src/corelib/text/qregularexpression.cpp: In lambda function:
|imx-yocto/build-xwayland-imx8mpsolidrun/tmp/work/x86_64-linux/qtbase-native/6.3.2-r0/git/src/corelib/text/qregularexpression.cpp:1194:17: error: lvalue required as unary ‘&’ operand
| return &dummySubject;
| ^~~~~~~~~~~~
| ninja: build stopped: subcommand failed.

Tags (2)
0 Kudos
Reply
3 Replies

218 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which product are you using?

0 Kudos
Reply

212 Views
tusharvernekar
Contributor II

i'am using imx8mpsolidrun board 

0 Kudos
Reply

195 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Can you try to clean all of this package and then rebuild it?

Here do you want to add the QT to the BSP? Our default BSP support QT6. 

0 Kudos
Reply