Issue with conga-QMX6 WEC7 image deployment from uSD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with conga-QMX6 WEC7 image deployment from uSD

980 Views
freescalewec7
Contributor I

Using a congatec conga-QMX6 SOM (PN: 016104, Quad), I am trying to load the stock WEC7 image (downloaded from Adeneo) onto a uSD and boot from it. I burned the eboot.nb0/NK.nb0 using cfimager, but upon boot the U-Boot console gives the following:

U-Boot 2009.08-00671-g5e573f0 QMX6Rx07 pn016104 (Jan 15 2014 - 14:20:15)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz

Temperature:   19 C, calibration data 0x5594d069

mx6q pll1: 792MHz

mx6q pll2: 528MHz

mx6q pll3: 480MHz

mx6q pll8: 50MHz

ipg clock     : 66000000Hz

ipg per clock : 66000000Hz

uart clock    : 80000000Hz

cspi clock    : 60000000Hz

ahb clock     : 132000000Hz

axi clock   : 264000000Hz

emi_slow clock: 132000000Hz

ddr clock     : 528000000Hz

usdhc1 clock  : 198000000Hz

usdhc2 clock  : 198000000Hz

usdhc3 clock  : 198000000Hz

usdhc4 clock  : 198000000Hz

nfc clock     : 24000000Hz

Board: i.MX6Q-QMX6: Board: 0x63012 [POR ]

Boot Device: SPI NOR

I2C:   ready

DRAM:   2 GB

MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2

JEDEC ID: 0xbf:0x25:0x4a

Reading SPI NOR flash 0xc0000 [0x2000 bytes] -> ram 0x27600ae0

*** Warning - bad CRC, using default environment

Reading SPI NOR flash 0x3fc000 [0x40 bytes] -> ram 0x275fff10

In:    serial

Out:   serial

Err:   serial

PFUZE100 Rev. 21 detected

Net:   got MAC address from IIM: 00:13:95:12:71:53

configure Atheros AR8035 Ethernet Phy

FEC0 [PRIME]

Hit any key to stop autoboot:  0

mmc0 is current device

** Partition 1 not valid on device 0 **

** Unable to use mmc 0:1 for fatload **

** Bad partition 1 **

mmc1(part 0) is current device

** Unable to use mmc 1:1 for fatload **

** Bad partition 1 **

Card did not respond to voltage select!

mmc2(part 0) is current device

MMC: block number 0x1 exceeds max(0x0)

** Can't read from device 2 **

** Unable to use mmc 2:1 for fatload **

** Bad partition 1 **

When a uSD with Linux is inserted, it boots correctly from mmc0 but it complains when it's loaded with WEC7 instead. Do I need to copy uboot, rootfs, etc. over to the uSD in order to have it boot properly? I'm not the most familiar with this U-boot configuration, so don't know if it's compatible to have U-boot run from SPI NOR. I also tried populating the uSD with a 6q_bootscript (dropping it into the FAT partition created during image burn) but it doesn't seem to find it (and truthfully the syntax may not be correct). I was hoping to be able to perform this activity without using MFG Tools (as I didn't want to permanently change the SPI NOR on the SOM and run anything outside of my control), but perhaps this is my only option.

Any thoughts would be greatly appreciated.

Labels (2)
0 Kudos
Reply
0 Replies