Issue with Network manager configuration in yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue with Network manager configuration in yocto

1,847件の閲覧回数
dkapure
Contributor I

I have a digi connectcore 8m nano SOM and I am trying to make a static eth0 configuration in yocto for the same. Following the instructions as specified in the official documentation 
(https://www.digi.com/resources/documentation/digidocs/embedded/dey/3.0/cc8mnano/yocto_t_configure-ne...

I have added the following lines in my local.conf 


ETH0_MODE = "static"
ETH0_STATIC_IP
= "192.168.0.2" ETH0_STATIC_NETMASK = "255.255.255.0" ETH0_STATIC_GATEWAY = "192.168.0.255"

 During building the image, the following error shows up


| readelf: Error: '/usr/lib/libjansson.so': No such file
| configure: error: Unable to locate the Jansson library
| WARNING: exit code 1 from a shell command.

Inspecting a few files, networkmanager_%.bb depends on the jansson package (libjansson.so), however, there was no such file found in the sysroot-native. 
Am I missing something here in the setup? or do I need to do some additional setup during the build?
TIA.

0 件の賞賛
返信
1 返信

1,817件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Please refer digi documents to check your steps

0 件の賞賛
返信