Issue with MIPI-DSI Connection on i.MX8M Plus - Framebuffer Not Created

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue with MIPI-DSI Connection on i.MX8M Plus - Framebuffer Not Created

2,126 次查看
kuri
Contributor III

Dear NXP Support,

I am currently working on connecting an LCD display via MIPI-DSI using the i.MX8M Plus. The MIPI-DSI is directly connected to the CPU, and I am using the ST7701 LCD. However, I have encountered the following errors:

[drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/bus@32c00000/mipi_dsi@32e60000 to encoder DSI-34: -19 imx_sec_dsim_drv 32e60000.mipi_dsi: Failed to attach bridge: 32e60000.mipi_dsi imx_sec_dsim_drv 32e60000.mipi_dsi: failed to bind sec dsim bridge: -19

Additionally, the following message is also being output related to this error:

drm_dbg_kms: No connectors found, will not create framebuffer!

This error might be causing dev->mode_config.num_connector to remain at 0, which in turn is likely causing the above message to be output within the drm_fbdev_client_hotplug function, leading to a situation where the framebuffer is not created.

I have attached the device tree, configuration files, and dmesg logs I am using. I would appreciate any advice on potential solutions for this issue.

Thank you for your support.

Best regards,

IMX8MPLUS 

 

0 项奖励
回复
2 回复数

2,090 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

This issue is due to hardware is not connected or bad driver, besides you dmesg don't mark an error you have to fix the driver.

Regards

0 项奖励
回复

2,076 次查看
kuri
Contributor III

Hi. @Bio_TICFSL ,

Thank you for your answer. 

Given that no errors are shown in the dmesg logs, it might indicate that the driver isn't functioning correctly and that there could be a missing configuration in the device tree. I suspect that it may be necessary to add information about the ST7701 to the mipi_dsi node. Is this addition required? If so, could you please provide any reference information that could assist?

&mipi_dsi

{

    status = "okay";

}

Best regards,

0 项奖励
回复