Issue with IMX219 Sensor Integration on Custom IMX8MP Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue with IMX219 Sensor Integration on Custom IMX8MP Board

394 次查看
Hardik_Prajapati
Contributor I

Hello,

I am currently working on integrating the IMX219 sensor with our custom IMX8MP board, using the ISP configuration.
We have ported the changes from the following repository into our custom Yocto layer: ( 6.6 sacrthgap KERNEL Version )
https://github.com/nxp-imx-support/meta-imx8mp-isp-imx219.

However, when running gst-launch-1.0 or v4l2-ctl commands, we are facing issues:

  • The pipeline captures the first frame with distortion but then gets stuck and does not proceed.

  • The image output is not proper.

Below are the details of our setup:

DTS configuration : 

&i2c3 {
	status = "okay";
	
	imx219: imx219@10 {
		compatible = "sony,imx219";
		reg = <0x10>;
		pinctrl-names = "default";
		pinctrl-0 = <&pinctrl_gpio_hog3>,<&pinctrl_gpio2>;
		clock-names = "xclk";
		clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
		assigned-clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;
		assigned-clock-parents = <&clk IMX8MP_CLK_24M>;
		assigned-clock-rates = <24000000>;
		mclk = <24000000>;
		mclk_source = <0>;
		csi_id=<0>;

		pwn-gpios = <&gpio1 1 GPIO_ACTIVE_HIGH>;
		
    		port {
		    imx219_to_mipi_csi2: endpoint {
		        remote-endpoint = <&mipi_csi_1_in>;
		        clock-lanes = <0>;
		        data-lanes = <1 2>;
			clock-noncontinuous;
		        link-frequencies = /bits/ 64 <456000000>;
  		    };
	       };
	};
};

&cameradev {
	status = "okay";
};

&mipi_csi_0 {
	#address-cells = <1>;
	#size-cells = <0>;
	status = "okay";
	port@0 {
		reg = <0>;
		mipi_csi_1_in: endpoint {
			remote-endpoint = <&imx219_to_mipi_csi2>;
			data-lanes = <2>;
			csis-hs-settle = <13>;
			csis-clk-settle = <2>;
			csis-wclk;
		};
	};
};

&isp_0 {
	status = "okay";
};

&isi_0 {
	status = "disabled";
};

&isi_1 {
	status = "disabled";
};

&dewarp {
	status = "okay";
};

 

Logs :

root@imx8mp-evk:~# dmesg | grep -E "csi| imx219"
[    0.046934] /soc@0/bus@30800000/i2c@30a40000/imx219@10: Fixed dependency cycle(s) with /soc@0/bus@32c00000/camera/csi@32e40000
[    0.047689] /soc@0/bus@32c00000/camera/csi@32e40000: Fixed dependency cycle(s) with /soc@0/bus@30800000/i2c@30a40000/imx219@10
[    0.056059] /soc@0/bus@30800000/i2c@30a40000/imx219@10: Fixed dependency cycle(s) with /soc@0/bus@32c00000/camera/csi@32e40000
[    0.059422] /soc@0/bus@30800000/i2c@30a40000/imx219@10: Fixed dependency cycle(s) with /soc@0/bus@32c00000/camera/csi@32e40000
[    0.062583] /soc@0/bus@32c00000/camera/csi@32e40000: Fixed dependency cycle(s) with /soc@0/bus@30800000/i2c@30a40000/imx219@10
[    0.065077] /soc@0/bus@32c00000/camera/csi@32e40000: Fixed dependency cycle(s) with /soc@0/bus@30800000/i2c@30a40000/imx219@10
[    0.065745] /soc@0/bus@30800000/i2c@30a40000/imx219@10: Fixed dependency cycle(s) with /soc@0/bus@32c00000/camera/csi@32e40000
[    0.065843] /soc@0/bus@32c00000/camera/csi@32e40000: Fixed dependency cycle(s) with /soc@0/bus@30800000/i2c@30a40000/imx219@10
[    1.930556] /soc@0/bus@32c00000/camera/csi@32e40000: Fixed dependency cycle(s) with /soc@0/bus@30800000/i2c@30a40000/imx219@10
[    1.942193] /soc@0/bus@30800000/i2c@30a40000/imx219@10: Fixed dependency cycle(s) with /soc@0/bus@32c00000/camera/csi@32e40000
[    5.841069] enter imx219_probe
[    5.869886] imx219 2-0010: No sensor reset pin available
[    5.871180] imx219_probe camera mipi imx219, is found
[    6.011700] mxc-md 32c00000.bus:camera: deferring csi device registration
[    6.062131] imx8_mipi_csi2_sam: module is from the staging directory, the quality is unknown, you have been warned.
[    6.085889] mxc-mipi-csi2-sam 32e40000.csi: supply mipi-phy not found, using dummy regulator
[    6.101666] : mipi_csis_imx8mp_phy_reset, No remote pad found!
[    6.107667] mxc-mipi-csi2-sam 32e40000.csi: lanes: 2, hs_settle: 13, clk_settle: 2, wclk: 1, freq: 500000000
[    6.577912] mx8-img-md: Registered sensor subdevice: imx219 2-0010 (1)
[    6.577925] mx8-img-md: created link [imx219 2-0010] => [mxc-mipi-csi2.0]
[    7.899921] scsi host0: usb-storage 1-1.2:1.0
[    8.938510] scsi 0:0:0:0: Direct-Access     SanDisk  Cruzer Blade     1.26 PQ: 0 ANSI: 6
[    9.205826] enter imx219_remove
[    9.438847] enter imx219_probe
[    9.445992] imx219 2-0010: No sensor reset pin available
[    9.455332] imx219_probe camera mipi imx219, is found
[    9.527424] mx8-img-md: Registered sensor subdevice: imx219 2-0010 (1)
[    9.536151] mx8-img-md: created link [imx219 2-0010] => [mxc-mipi-csi2.0]
[   10.501160] scsi host0: usb-storage 1-1.2:1.0
[   11.527747] scsi 0:0:0:0: Direct-Access     SanDisk  Cruzer Blade     1.26 PQ: 0 ANSI: 6

 

Pipeline Behavior and Logs During Capture: Command:

root@imx8mp-evk:~# gst-launch-1.0 v4l2src device=/dev/video2 ! videoconvert ! autovideosink sync=false                                                                      
[  239.695562] enter isp_mi_stop
[  239.891296] enter isp_mi_stop
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
[  240.400653] enter isp_mi_stop
[  240.451547] enter isp_s_comp
[  240.454467] enter isp_s_comp
[  240.457462] enter isp_s_comp
[  240.480579] enter wdr3_hw_init
[  240.483684] wdr3 res: 1920 1080 
[  240.487183] enter isp_s_comp
[  240.539054] enter isp_set_stream 1
[  240.554111] enter isp_mi_start
Redistribute latency...
0:00:10.8 / 99:99:99.

 

OUTPUT :
shared image.jpeg

Media Ouput :

root@imx8mp-evk:~# media-ctl -p
Media controller API version 6.6.74

Media device information
------------------------
driver          mxc-md
model           FSL Capture Media Device
serial          
bus info        platform:32c00000.bus:camera
hw revision     0x0
driver version  6.6.74

Device topology
- entity 1: mxc-mipi-csi2.0 (8 pads, 1 link)
            type Node subtype V4L flags 0
            device node name /dev/v4l-subdev0
        pad0: Sink
                <- "imx219 2-0010":0 [ENABLED,IMMUTABLE]
        pad1: Sink
        pad2: Sink
        pad3: Sink
        pad4: Source
        pad5: Source
        pad6: Source
        pad7: Source

- entity 10: imx219 2-0010 (1 pad, 1 link, 0 routes)
             type V4L2 subdev subtype Sensor flags 0
             device node name /dev/v4l-subdev1
        pad0: Source
                [stream:0 fmt:SRGGB10_1X10/1920x1080 field:none]
                -> "mxc-mipi-csi2.0":0 [ENABLED,IMMUTABLE]

 

I would appreciate any assistance or suggestions on how to resolve this issue.

Thanks & Regards,
Hardik

0 项奖励
回复
1 回复

379 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Apparently you have to change the clock rate, I don't have your sensor at hand but iMX219 is very used with MX8MP.

regards

0 项奖励
回复