Issue regarding the IMXRT1170 PIT timer and eDMA transfer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue regarding the IMXRT1170 PIT timer and eDMA transfer

776 Views
Sanjay1993
Contributor I


Board: MIMXRT1170-EVK
Core: M4
We are working on LPSPI_DMA with PIT timer for delay between transfer. We were not able to attain the required output by using the PIT 1 channel 1 using eDMA Channel 1.
We used peripherals for enabling the periodic trigger and we were not able to get the data transfer for SPI. Please give us a solution regarding the issue.

Labels (1)
0 Kudos
Reply
1 Reply

769 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Sanjay1993 ,

  Do you want to use the PIT to trigger the LPSPI data transfer, and LPSPI data transfer use the DMA right?

  If yes, you can use the PIT generate the interrupt, then trigger the LPSPI transfer, then use the LPSPI DMA transfer.

  About the code, you can refer to the SDK:

\SDK_2_10_0_MIMXRT1170-EVK\boards\evkmimxrt1170\driver_examples\lpspi\edma_b2b_transfer

SDK_2_10_0_MIMXRT1170-EVK\boards\evkmimxrt1170\driver_examples\pit\cm7

 

Wish it helps you!

If you still have questions about it please kindly let me know.

Best Regards,

Kerry

0 Kudos
Reply