Issue in setting WiFi DTB file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue in setting WiFi DTB file

1,402件の閲覧回数
devikar
Contributor II

Hi,

We have setup Yocto project 4.9.11_1.0.0 on a imx6qpsabresd based custom board which has murata wifi module LBWA1KL1FX-875.
We have followed the steps from murata organisation to build the output.On bootup we have to set fdt_file as imx6qp-sabresd-btwifi.dtb.
We have flashed the output files using mfgtool.
We have followed the below mentiones step on bootup.

-> setenv fdt_file imx6qp-sabresd-btwifi.dtb
-> saveenv
-> printenv fdt_file
-> fdt_file=imx6qp-sabresd-btwifi.dtb
-> bootup
-> switch to partitions #0, OK
mmc2(part 0) is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
7119312 bytes read in 203 ms (33.4 MiB/s)
Booting from mmc ...
reading imx6qp-sabresd-btwifi.dtb
** Unable to read file imx6qp-sabresd-btwifi.dtb **
Kernel image @ 0x12000000 [ 0x000000 - 0x6ca1d0 ]
No gpc device node -9, force to ldo-enable.

Starting kernel ...


It is failing to read imx6qp-sabresd-btwifi.dtb file.
Please let us know what could be the issue.

Thanks,
Devika

ラベル(3)
0 件の賞賛
返信
1 返信

1,334件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Devika

one can try to rebuild imx6qp-sabresd-btwifi.dtb with LBWA1KL1FX-875

firmware from scratch :

Yocto Training - HOME 
[meta-freescale] dts and dtb files 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信