Issue in flashing u-boot from MFGTool on custom board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue in flashing u-boot from MFGTool on custom board

2,919 次查看
sadasivappasidd
Contributor I

Hi, 

My customer board u-boot was corrupted due to incorrect u-boot flashing from update procedure. Now board is not booting. So i am using MFGTool to re-flash my default u-boot to board. But u-boot loading will stop at the midway, We are not able to identify the reason that causing this abort at midway.

Any thoughts regarding this?

Please find attached screenshots of the MFGTool while flashing the u-boot.

标签 (3)
0 项奖励
回复
1 回复

2,643 次查看
igorpadykov
NXP Employee
NXP Employee

Hi sadasivappa

for custom board it is necessary to run ddr test

i.MX6/7 DDR Stress Test Tool V2.80 

and rebuild mfg tool firmware (files in /firmware folder)

with new calibration coefficients set in uboot/../freescale/board/board_name/*.cfg

file. Please use sect.6.2 Manufacturing Tool, MFGTool attached Yocto

Guide. Use corresponding mfg tools version the same as bsp version from link

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复