Issue in enabling LCDIF clock at uboot level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue in enabling LCDIF clock at uboot level

2,141 Views
sd05
Contributor III

We are having a imx8m mini based customboard we want to port  MIPI DSI based st7703 lcd panel driver at uboot and display splash screen.

1. We are able to port the st7703 driver (taking  reference of rm67191 driver) with uboot 2020 version for our board as well. Probe is getting call and please see the logs, video-link is being created with lcdif, video bridge and panel.

2. Since the mipi panel is already working in the kernel, so we kind of ported the clock values as well. But as attached in clk-dump the usecnt is 0 for all the display related clocks.

3. We also see in imx8mm.dtsi file there is display-subsystem node, whose compatible string matches with the drm core. But in uboot we do not have support for it. Do we need to add that?

Currently everything is working fine, but somehow the clock is not getting init. We also probed the hardware and we do not see the clk with the probe too

 

0 Kudos
Reply
1 Reply

2,136 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sunidhi

 

for uboot mipi-dsi usage one can look at

https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8mm_evk/imx8mm_evk.c?h=...

 

Best regards
igor

0 Kudos
Reply