Issue in capturing images over MIPI-CSI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue in capturing images over MIPI-CSI

ソリューションへジャンプ
2,906件の閲覧回数
namanthaker
Contributor IV

Hello,

I am integrating a third party ISP and Camera Sensor on i.MX8M Mini EVK over MIPI-CSI. I have integrated a driver into Yocto L5.4.47-2.2.0 and I am observing data and clock on the MIPI lines from ISP+Sensor. But I am unable to capture any images on i.MX8MM side.

Gstreamer command used to capture the image:
gst-launch-1.0 -v v4l2src device="/dev/video0" num-buffers=1 ! 'video/x-raw, width=(int)640, height=(int)480, format=(string)UYVY' ! jpegenc ! filesink location=/home/root/test.jpg

The gstreamer waits for capturing an image but nothing is recevied. When I press Ctrl+C and check the file size, it comes out zero i.e there is no data in the captured image. Also, gstreamer does not give any errors in the log.

The ISP+Sensor combo transmits image in YUV422 format and I am seeing MIPI CSI interrupts in /proc/interrupts.
root@imx8mmevk:~# cat /proc/interrupts | grep -i mipi_csi
57: 147901 0 0 0 GICv3 49 Level 32e30000.mipi_csi

Q1. To debug this, I want to dump the low level framebuffer data from MIPI-CSI receiver driver so that I can confirm whether the MIPI CSI reciever driver is capturing the data or not.
Is this possible? If yes, then how do I dump the framebuffer data from driver level closest to MIPI HW?

Q2. I also tried to read the MIPI CSI registers 0x32E3_0004 to 0x32E3_011C using devmem utlity, but the system hangs when I try to read these registers.
I am able to read other registers like 'SNVS_HP Version ID Register 1' successfully using this utlity.
Is there any other way to read the MIPI CSI registers to find out its status?

Q3. Is there is any other way to confirm if the frames are correctly captured by the MIPI-CSI interface? Any further debug points to help will be very much appreciated.

Regards,
Naman

ラベル(1)
0 件の賞賛
返信
1 解決策
2,841件の閲覧回数
namanthaker
Contributor IV

Hi @joanxie ,

I apologise for the late response.

I got the CSI capturing working by using 2-lanes configuration. The issue seems to be with 4-lane configuration only. When I am using 4-lanes, I am unable to capture anything. For this 4-lane issue, I have raised another query.

I got UYVY working by adding the format support in the core drivers by taking reference from another IMX8MM based system which has same ISP+Sensor support which I am trying to integrate.

Regards,
Naman

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
2,636件の閲覧回数
jfontain88
Contributor II

Hi,

I encounter exactly the same issue from the original post but i can't see how you resolved it @namanthaker  What did you change? By trying with 1, 2 and 4 lanes nothing can get me valid frames...

Am working on another sensor but the issue is the same: drivers recognize devices, device tree updated but gstreamer stuck on set_stream and i am forced to ctrl+C to abort it and size of my output file is 0. I wonder that it is a clock problem? data format problem? etc...? How did you resolve your case please @namanthaker ? Anyone knows the solution to this type of problem or maybe is it better to create a new post for my problem?

Thanks a lot !

0 件の賞賛
返信
2,575件の閲覧回数
namanthaker
Contributor IV

Hi @jfontain88,

I had issue only while using 4-lane. When DTS and sensor were configured for 2-lane or 1-lane everything was working fine. Afterwards it was found that the problem with 4-lane was setup related i.e. problem with copper wire connection between IMX8MM EVK and sensor EVM. I disassembled the entire setup and recreated the setup with new copper wires. I also used a clean SW build with the kernel changes suggested in below query:
https://community.nxp.com/t5/i-MX-Processors/Issue-with-using-MIPI-CSI-4-Lane-on-i-MX8MM/m-p/1287968...

Could you try the 4-lane patch in the above query and check if it helps?

Regards,
Naman

2,563件の閲覧回数
jfontain88
Contributor II

HI,

 thank you very much for your reply but i still can't get data even from 1, 2 or 4 lanes. I think that my problem is not the same as yours then

I'll work on it. Thanks a lot!

0 件の賞賛
返信
2,860件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
2,842件の閲覧回数
namanthaker
Contributor IV

Hi @joanxie ,

I apologise for the late response.

I got the CSI capturing working by using 2-lanes configuration. The issue seems to be with 4-lane configuration only. When I am using 4-lanes, I am unable to capture anything. For this 4-lane issue, I have raised another query.

I got UYVY working by adding the format support in the core drivers by taking reference from another IMX8MM based system which has same ISP+Sensor support which I am trying to integrate.

Regards,
Naman

0 件の賞賛
返信
2,826件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I have replied to you in your another 4-lane issue case, did you have any issue about this case?

0 件の賞賛
返信
2,806件の閲覧回数
namanthaker
Contributor IV

Hi @joanxie ,

There is no more issue with this query. I have marked my previous reply as solution to close this query.

Regards,

Naman

0 件の賞賛
返信
2,867件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

did you get any wrong message? it seems doesn't support UYVY, how about testing by

"gst-launch-1.0 v4l2src device=/dev/video0 num-buffers=1 ! jpegenc ! filesink location=test.jpg" ?

what registers of you mean " 0x32E3_0004 to 0x32E3_011C"?

0 件の賞賛
返信