Unable to enable clock for HDMI TX in IMX8QM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to enable clock for HDMI TX in IMX8QM

815 Views
vinothkumars
Senior Contributor IV

Hi,

 

I am working on HDMI TX for IMX8QM Custom variant with Android.

 

I got kernel crash because of following functionality from dts,

 

clk_gate2_scu_is_enabled:

 

clks[IMX8QM_HDMI_LIS_IPG_CLK] = imx_clk_gate2_scu("hdmi_lis_ipg_clk", "ipg_hdmi_clk_root", LPCG_ADDR(DI_HDMI_LPCG + 0x4), 16, FUNCTION_NAME(PD_HDMI));
clks[IMX8QM_HDMI_MSI_HCLK] = imx_clk_gate2_scu("hdmi_msi_hclk_clk", "ipg_hdmi_clk_root", LPCG_ADDR(DI_HDMI_LPCG + 0x14), 0, FUNCTION_NAME(PD_HDMI));
clks[IMX8QM_HDMI_PXL_LPCG_CLK] = imx_clk_gate2_scu("hdmi_pxl_lpcg_clk", "dummy", LPCG_ADDR(DI_HDMI_LPCG + 0x18), 0, FUNCTION_NAME(PD_HDMI));
clks[IMX8QM_HDMI_PXL_EVEN_CLK] = imx_clk_gate2_scu("hdmi_pxl_even_clk", "hdmi_pxl_lpcg_clk", NULL, 0, FUNCTION_NAME(PD_HDMI));
clks[IMX8QM_HDMI_HDP_CLK] = imx_clk_gate2_scu("hdmi_pxl_odd_clk", "hdmi_pxl_lpcg_clk", NULL, 0, FUNCTION_NAME(PD_HDMI));
clks[IMX8QM_HDMI_PXL_DBL_CLK] = imx_clk_gate2_scu("hdmi_pxl_dbl_clk", "hdmi_pxl_lpcg_clk", NULL, 0, FUNCTION_NAME(PD_HDMI));
clks[IMX8QM_HDMI_VIF_CLK] = imx_clk_gate2_scu("hdmi_vif_clk", "hdmi_pxl_mux_clk", LPCG_ADDR(DI_HDMI_LPCG + 0x1C), 0, FUNCTION_NAME(PD_HDMI));
clks[IMX8QM_HDMI_APB_CLK] = imx_clk_gate2_scu("hdmi_apb_clk", "ipg_hdmi_clk_root", LPCG_ADDR(DI_HDMI_LPCG + 0x28), 16, FUNCTION_NAME(PD_HDMI));
clks[IMX8QM_HDMI_APB_MUX_CSR_CLK] = imx_clk_gate2_scu("hdmi_apb_mux_csr_clk", "hdmi_apb_clk", LPCG_ADDR(DI_HDMI_LPCG + 0x20), 16, FUNCTION_NAME(PD_HDMI));
clks[IMX8QM_HDMI_APB_MUX_CTRL_CLK] = imx_clk_gate2_scu("hdmi_apb_mux_ctrl_clk", "hdmi_apb_clk", LPCG_ADDR(DI_HDMI_LPCG + 0x24), 16, FUNCTION_NAME(PD_HDMI));
clks[IMX8QM_HDMI_HDP_PHY_CLK] = imx_clk_gate2_scu("hdmi_pclk", "ipg_hdmi_clk_root", LPCG_ADDR(DI_HDMI_LPCG + 0x1C), 16, FUNCTION_NAME(PD_HDMI));

 

clk_gate_scu_enable

 

 clks[IMX8QM_HDMI_I2C0_CLK] = imx_clk_gate_scu("hdmi_i2c0_clk", "hdmi_i2c0_div", SC_R_HDMI_I2C_0, SC_PM_CLK_MISC2, LPCG_ADDR(DI_HDMI_LPCG), 0, 0);

 

 

 

Regards,
Vinothkumar Sekar
0 Kudos
Reply
0 Replies